Subject | Author | Posted | |
---|---|---|---|
Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2. The X-STM32MP-GNS...
| 2024-11-12 3:33 AM | ||
i am planning to build an dpoae device so which one do u prefer STM32MP157D-DK1 processor or STM32H...
| 2024-09-18 12:08 AM | ||
Hello everyone,
I am trying to program the STM32MP157 to control a simple LED using Keil software...
| 2024-09-15 5:30 AM | ||
Hi, i am facing the issue with the header file like I am using ADC pin where i facing the issue wi...
| 2024-09-03 5:11 AM | ||
NOTICE: CPU: STM32MP157FAC Rev.Z NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board...
| 2024-08-20 12:14 AM | ||
Hello STM Community, I am considering using the STM32MP157F-DK2 as a platform for a LoRa gatewa...
| 2024-07-25 10:27 PM | ||
Good afternoon.
I observe very strange behavior when the first few images received from the camer...
| 2024-07-01 6:25 AM | ||
Dear STM32 Forum Community,
I am currently working with the STM32MP157F-DK2 development kit and h...
| 2024-06-18 10:17 PM | ||
Hi there, I'm trying to integrate in my linux distribution (custom board based on STM32MP153) a L...
| 2024-04-22 2:49 AM | ||
*I've imported successfully of STM32mp157 dk-1 board 's schematics in altium designer and I don...
| 2024-04-08 6:03 AM | ||
Hello, We are currently working with the STM32MP157F-DK2 board and the on-board SDRAM (DDR3L). The...
| 2024-04-04 9:47 AM | ||
Hi, I'm please to share we pass extensive validation test of Zentel Japan 4Gb DDR3 A3T4GF40BBF-HP...
| 2024-03-22 7:35 AM | ||
Hello, we are currently working with the STM32MP157F-DK2 evaluation board. We have a couple questio...
| 2024-03-05 8:19 AM | ||
Hello, I'm trying to boot my EVAL board with the images from STM32MP1 Starter package version 5...
| 2024-02-14 12:51 AM | ||
I have an STMP157F-EV1 and I have followed the instructions here to download and program the starte...
| 2024-01-25 11:39 AM | ||
Hello! I'm trying to figure out if the M4 has the ability to put the A7 to sleep but haven't quite...
| 2023-11-28 9:42 AM | ||
Hey all, I'm trying to test DRM/KMS on an STM32MP1 board, but I can't do this while weston is takin...
| 2023-09-18 3:28 PM | ||
i have download the embedded wizard example from https://www.embedded-wizard.de/platforms/stmicroel...
| 2023-09-15 2:28 AM |