Subject | Author | Posted | |
---|---|---|---|
I am trying to debug a simple application on the CM4 processor on a STM32MP157D-DK1 development boa...
| 2025-05-06 4:40 AM | ||
hello, i have an issue trying to install QT expansion package on stm32MP257F-DK2 with openstlinux ...
| 2025-05-01 9:02 AM | ||
Moved from MCUs forum. I met this error and can not continue flashing the board. Could any o...
| 2025-04-23 6:04 AM | ||
Hello ST Team, We are planning to use the STM32MP2 series MPU in one of our design. We have found ...
| 2025-04-22 9:43 PM | ||
Hello, We recently bought an STM32MP257f-dk board. We are running OpenSTLinux on it. We would l...
| 2025-04-22 5:59 AM | ||
The board seems to be very selective on the power provided on the STLINK port. Even with an USB 2.0...
| 2025-04-11 4:56 AM | ||
Hi, And currently using the STM32MP157F-DK2 demonstration board using Open ST Linux (Kirkstone). ...
| 2025-04-11 4:18 AM | ||
Found the cause and solved. what happened was: 1. Plugged the host PC only into the STLINK USB-C. ...
| 2025-03-19 11:38 PM | ||
[1] Why is the STM32MP257 called STM32 and not STM64 :) for 64 bit ? [2] What is the reason th...
| 2025-03-12 7:40 AM | ||
Hi, I am debugging STM32MP2 via JTAG and would like to access a process via DAP. I believe it i...
| 2025-03-10 7:01 PM | ||
I need to migrate my project from STM32MP135F-DK board to custom hardware (SoM based on STM23MP135D...
| 2025-02-27 3:02 AM | ||
Hello, I have a custom board based on STM32MP257F-EV1 but with an eMMC (4 bits) connected on SDMM1...
| 2025-02-14 8:42 AM | ||
Hi, im planing on running computer vision DL models on multiple STM32 boards. At this moment I will...
| 2025-02-14 5:55 AM | ||
After my video data is encoded by H264 hardware, the picture becomes darker. This issue doesn't occ...
| 2025-02-12 12:10 AM | ||
Hello, For students, we recently bought the STM32MP257F eval board, and the related camera and hdm...
| 2025-02-07 5:49 AM | ||
Hi I'm new to embedded software development and STM32 too.I'm just wanna learn and explore everyth...
| 2025-02-04 9:41 PM | ||
I have a STM32MP257F-DK board and am using the OpenSTLinux image. I want to use the USB C connector...
| 2025-01-31 3:50 PM | ||
While reviewing the schematic of the STM32MP157 EVAL development board, I came up with the foll...
| 2025-01-26 4:14 AM | ||
We have a board with PMIC attached to I2C2. I've followed the directions in https://wiki.st.com/stm...
| 2025-01-19 8:42 PM | ||
Using OSTL 4.1.2 and build DISTRO=openstlinux-weston MACHINE=stm32mp15-disco on STM32MP157F-DK2. Fo...
| 2024-12-24 11:52 PM |