| Subject | Author | Posted | |
|---|---|---|---|
|
Hi team. I'm using ADC injected channel conversion with PWM for BLDC motor control. I would like ...
| 2024-04-25 8:57 AM | ||
|
I'm trying to control a PMSM motor using Nucleo-G474RE and STEVAL-IHM023V3 motor control boards and...
| 2024-04-21 10:24 PM | ||
|
I want to display the current updates, speed, and voltage of the motor on an ST7735 display. I'm fa...
| 2024-04-18 12:11 AM | ||
|
Hello, I have intsalled the motorbench version 6.2.1, and I have already the cubeMX version 6.9, b...
| 2024-04-17 1:16 AM | ||
|
Hi I am struggling with the appearance of my BEMF in my 6 step control. The picture shows one of ...
| 2024-04-12 3:59 AM | ||
|
Hello, I am working on a motor control project that is to be driven battery-powered. This means...
| 2024-04-08 6:05 AM | ||
|
If I get the Ke from motor profiler,how do I calculate the torque constant (Kt)?
How do I calcula...
| 2024-04-02 3:49 AM | ||
|
I want to control the speed of an AC motor with STM32, using pin PA6 on the MCU as an external inte...
| 2024-03-23 12:46 AM | ||
|
I am essentially experiencing the exact same issue as this poster. I have a single conversion ...
| 2024-03-22 10:09 AM | ||
|
Good day sir, i want to ask about pwm duty cycle sir. I have a coustem board with input 220vac, aft...
| 2024-03-19 6:38 PM | ||
|
Hello. Our goal is to create a medical motor control program used to cut bones. For this purpose,...
| 2024-03-19 12:44 AM | ||
|
#include "main.h"
#include "stdlib.h"
#include "string.h"
#include "math.h"
#include "ctype.h"
#inc...
| 2024-03-19 12:30 AM | ||
|
Hello, I do have a problem running STM32 Motor Control Workbench 6.2.1 . The UI doesn't load at a...
| 2024-03-15 2:46 AM | ||
|
1.Using the STSPIN4G chip, after enabling the timer output, an error message will be reported stati...
| 2024-03-08 2:00 AM | ||
|
I have made a custom 24V drive using the STSPIN32F0 chip. For the first take on this board, I have ...
| 2024-03-05 12:00 PM | ||
|
I am trying to drive a 250W BLDC motor. I started profiling the motor, which looked promesing. I ba...
| 2024-03-04 2:19 AM | ||
|
Dear support, I am designing a ACIM driver. I want to change MCU to 48 pin LQFP package. but examp...
| 2024-02-28 8:58 AM | ||
|
Hello ST,
we are working with B-G431-esc development tool to control motor. When we worked with y...
| 2024-02-28 12:51 AM | ||
|
Good day all. I want to learn about mc worckbech. I want to coustem with mcu STM32f401 and a part...
| 2024-02-26 1:12 AM | ||
|
Hi. I m new at ST MCSDK and i was reading some documents about mcsdk position control until waitin...
| 2024-02-26 12:33 AM |