Subject | Author | Posted | |
---|---|---|---|
Hi Everyone, Sorry for being quiet this past few weeks! I've been involved in doing some interna...
| 2019-10-31 5:37 AM | ||
Hello, The datasheet for the STMF746G dev board has a camera connector (P1), which by the datash...
| 2019-10-30 8:53 AM | ||
is there some solution to choose? easy to store video data , and detect fatigue
| 2019-10-22 6:22 PM | ||
Hi all, I have a requirement of using a TFT LCD. Here the input to the Controller will be coming ...
| 2019-10-16 11:44 PM | ||
I need draw a curve to display the sensors readings. The curve contains dots and lines. I created...
| 2019-10-16 10:56 AM | ||
Now that the h/w jpeg decode is working so well I have turned my attention to the encode side. I'm ...
| 2019-10-13 3:02 AM | ||
I capture an image using the ov9655 camera module. The selected the image format as rgb565. The ima...
| 2019-10-02 3:54 AM | ||
Hi What is the easiest way to interface a camera. AN5020 lists a number of camera sensors suppor...
| 2019-10-01 6:17 AM | ||
We are using a STM32H743I-EVAL2 and have our LCD frame buffers running on SDRAM1 using the FMC. On...
| 2019-10-01 6:10 AM | ||
2019-10-01 4:54 AM | |||
Does anyone know of a driver for ILI9806 over DSI. Best regards Thomas
| 2019-09-30 11:59 PM | ||
Hi, i am using STM32F407 in which i create a website using ssi and cgi handlers now i want to displ...
| 2019-09-23 6:38 AM | ||
Hi, we have custom board based on stm32f769 and ov2640 camera configured to jpeg output at 160x12...
| 2019-09-18 12:30 AM | ||
I'm using the TEXT widget. How do you view a changing variable? The variable is changed by a counte...
| 2019-09-16 4:54 AM | ||
Is there a way I can control SDRAM refresh to occur during frame blanking using LTDC and FMC on a S...
| 2019-09-12 3:04 AM | ||
Working on STM32F746G-Disco board, my app works on board, simulator compiles on Visual Studio, but ...
| 2019-09-12 1:31 AM | ||
Hi all, I`m trying to build a project with STM32CubeMX , Using FATFS for SDcard and Decoding JPE...
| 2019-09-12 12:38 AM | ||
Hi all, I`m trying to build a project with STM32CubeMX , Using FATFS for SDcard and Decoding JPE...
| 2019-09-12 12:36 AM | ||
We are facing issues in compiling STemWin has windows.h headers are not found, below is the log for...
| 2019-09-11 11:35 PM | ||
I am using STM32F469 for my project. Also, I want to interface 1.54" TFT LCD with it. I used CubeM...
| 2019-09-08 11:38 PM |