Subject | Author | Posted | |
---|---|---|---|
I am considering STM32W MCU for capturing images from an image sensor, such as the OV7725 or OV7670...
| 2020-01-08 2:46 PM | ||
Hi community, We're getting our image from a buffer containing 8bits-values (array of chars). Du...
| 2020-01-08 5:35 AM | ||
Dear Friends, I would like to appreciate the effort of STM for providing user friendly software ...
| 2020-01-07 10:35 PM | ||
Hi guys, For those of you that have been on holiday, i hope you had a good time. We're finally b...
| 2020-01-06 1:04 AM | ||
I am working with STM32F746NGHx. I am using STM32Cube, System Workbench and TouchGFX Designer. ...
| 2020-01-02 5:56 AM | ||
Hello, So i did try to port my project to the STM32H747I-DISCO board, to evaluate if possible t...
| 2020-01-01 7:15 AM | ||
Hello, The datasheet for the STM32WB55 says that the STM32WB55Rx (the VFQFPN68 version) has 4x28...
| 2019-12-28 4:44 PM | ||
My first simplest touchGFX application can run on my st board. Now, I changed some UI with Desig...
| 2019-12-26 12:25 AM | ||
Hi All, I need your help , I am configuring TouchGFX with DSI ( STM32F778AI ) with RM67162 360X320...
| 2019-12-24 2:41 AM | ||
My HW_Init.cpp is as follows. How do I modify the LCD display orientation?
| 2019-12-21 5:57 PM | ||
In my final design, I will have an SD Card to read/write to. When running in the simulator, is ther...
| 2019-12-20 10:33 PM | ||
Hi all, I have this Eclipse related error on CubeIDE that is very bizarre and any help for it wo...
| 2019-12-20 10:25 PM | ||
Visual Studio compiles the simulation project generated by TouchGFX. See attachment for error messa...
| 2019-12-20 8:50 PM | ||
Hello, I would like to reverse the screen orientation on the Hello World example for STemWin pr...
| 2019-12-20 7:43 AM | ||
2019-12-20 6:17 AM | |||
I see that in G0 G4 Folder STM32Cube\Repository\STM32Cube_FW_G0_V1.3.0\Middlewares\ST STemWin is mi...
| 2019-12-17 8:50 AM | ||
Hi, I'm getting transfer error from DMA interrupt by the attempt to get image from the DCMI. ...
| 2019-12-17 7:44 AM | ||
After compilation, I cannot program STM. An error appears. Why? make: *** No rule to make target...
| 2019-12-16 10:32 AM | ||
Hello there, I have a custom board for STM32F429BIT6 and want to setup a 7inch AT070TN94 LCD in...
| 2019-12-13 11:34 PM | ||
2019-12-13 1:38 AM |