Subject | Author | Posted | |
---|---|---|---|
Hi, Consider the following two CustomContainers and the Screen class : class CustomContainer : ...
| 2020-09-30 05:10 AM | ||
Hello, I have some doubt regarding touchgfx Suppose I set for Double buffer and I am using cust...
| 2020-09-29 11:23 PM | ||
I want to play a video on 7" (800x480) TFT via ft810. I couldn't decide the mcu for this. STM32 Do...
| 2020-09-23 06:07 AM | ||
Hey guys. I need to have a HMI in my project. I decided to use touchgfx . My question is that ca...
| 2020-09-22 10:27 AM | ||
2020-09-22 12:53 AM | |||
Dear all, on several Discovery boards of the STM32L4/5 series the above mentioned display is used....
| 2020-09-18 06:34 AM | ||
Hello, I've a smal implementation for the STM32L073 without using of the HAL. For the configurati...
| 2020-09-18 03:22 AM | ||
Hello there, for my master thesis I am trying to receive data over DCMI with the STM32H742. As an ...
| 2020-09-18 02:02 AM | ||
Does LTDC access memory outside the scope of each layer? Example Screen: 800x600 Layer 1: (...
| 2020-09-16 10:16 PM | ||
just simply read the code in /touchgfx/target , for not all HAL function ,could not find a resp...
| 2020-09-16 05:52 PM | ||
Hello. Is there a better way to rotate image by 90 degree than just decompress into pixel array and...
| 2020-09-15 11:57 AM | ||
Hi all. I am currently working on a project using my STM3220G board with a 3.2 " TFT and STemWin. I...
| 2020-09-10 07:01 AM | ||
Hi It seems that ChromART supports A4 and A8 formats very well, but I haven't found a way to dra...
| 2020-09-08 11:54 PM | ||
Hello, I don't know what is the problem with my project but when I try to update graph the screen ...
| 2020-09-08 08:36 PM | ||
systme is TW2835 with stm32h747 i catch video data but DCMI->DR cannot write to sdram buffer w...
| 2020-09-08 01:57 AM | ||
Greetings, today I tried generating a VGA hsync and vsync signal using PWM on my NUCLEO-H743ZI2. T...
| 2020-09-07 02:19 PM | ||
Hello, I've got a strange bug at times when clicking on a 'home-made' button. VS stops at SDL_Dest...
| 2020-09-07 05:52 AM | ||
Hi All, Recently, i have testing memory device Because of the flickering. I've attached my ap...
| 2020-09-04 04:01 AM | ||
Hello Team, I've a 64MB flash from custom board. I able to flash JPEG hex array to Flash sectio...
| 2020-09-02 07:14 AM | ||
I have STM32F407vg and 3.2" Touch Screen TFT LCD Module - ILI9325 like this: https://www.hotmcu.co...
| 2020-09-01 08:01 AM |