| Subject | Author | Posted | |
|---|---|---|---|
|
Hello, I am blocked with a personnal project using a STM32F769I-DISCO, TouchGFX and audio: DMA ...
| 2025-08-14 11:03 PM | ||
|
Hello community! On March 18, we launched a TouchGFX Contest that had for goal for us to see our...
| 2025-07-07 6:23 AM | ||
|
Hello all, I have issue of Touch GFX post generate target error of unable to locate file. I am usi...
| 2025-04-23 1:37 AM | ||
|
Hello, I am using the STM32U5G9J-DK1 to learn the GUI development, and I have created a very simpl...
| 2025-04-14 12:19 PM | ||
|
In the E-Bike Demo, inside LanguageSelector.cpp (Container) there's the function void LanguageSel...
| 2025-04-11 3:43 AM | ||
|
Hi! I have an issue with one of my implementations. void CalendarRepetitiveDaysView::scroll...
| 2025-04-11 1:00 AM | ||
|
Sometimes I want a source folder in Windows set to case sensitive so I can fix the case of filename...
| 2025-04-10 9:17 AM | ||
|
I need suggestion to implement continous sine wave sound and drive spi based screen. I use DMAs for...
| 2025-03-27 6:23 AM | ||
|
Hello, I'm developing graphics on an STM32H750-based board using TouchGFX, and my framebuffer is l...
| 2025-03-21 7:42 AM | ||
|
Hello, I'm currently developing graphics on an STM32H750-based board using TouchGFX, and my frameb...
| 2025-03-18 4:15 AM | ||
|
Using Touchgfx at the same time with writing to external QuadSPI-Flash was not possible, because fo...
| 2025-03-13 7:36 AM | ||
|
Can some one help me with this to integrate graphic.
Step By Step Guide path included. LVGL g...
| 2025-03-03 3:44 AM | ||
|
Hello! I've been having some problems to update a flex button inside a custom container that i c...
| 2025-02-26 5:17 AM | ||
|
Hi, I'm facing an issue displaying an image on a 1024x600 screen via RGB. As shown in the image, t...
| 2025-02-12 4:41 AM | ||
|
MCU: STM32U575VG TFT with embedded RAM: 16bpp, 8-bit 8080 interface I'm following this scheme in ...
| 2025-02-11 8:33 AM | ||
|
Does anybody know a graphics library that is "mostly" Misra compliant? Then is there a graphics so...
| 2025-02-11 1:27 AM | ||
|
Dear Community, We have seen many threads asking whether TouchGFX supports multitouch. To addres...
| 2025-02-04 2:08 AM | ||
|
Hi, i am using linux and want to customise STM32U5A9 discovery kit display. I am not able to use to...
| 2025-01-30 10:06 PM | ||
|
I am working on a project that needs to integrate a 240x240-round display. The display uses a GC9A0...
| 2025-01-04 9:05 PM | ||
|
BKPT will be inserted with arm compiler 6.22 . The program does not automatically run down....
| 2024-11-26 7:19 PM |