cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-DISPLAY with Half-Duplex SPI

sbaker
Associate II

I am attempting to use the X-CUBE-DISPLAY module generated from STM32CubeMX for a ST7789V display. The configuration requires the selection of the LCD BUS IO driver to be a SPI port in Full-Duplex Master mode. However my display only has a single SDA line for input and output, so the SPI has to be configured in Half-Duplex Master mode. X-CUBE-DISPLAY will not allow this SPI port to be selected, so the code generation fails.

Is there a way for the X-CUBE-DISPLAY to work with a half-duplex SPI peripheral? 

0 REPLIES 0