Subject | Author | Posted | |
---|---|---|---|
Hello Community, I am using the driver L99DZ100GP as SBC in one of our projects. We have configure...
| 2023-08-18 7:08 AM | ||
Hello all, I am new to embedded programming and I am practicing embedded program and trying out...
| 2023-08-09 11:41 AM | ||
I am trying to implement the BLE stack (WB5 series) on an RTOS. I work with stm32wb5mm-dk evaluatio...
| 2023-08-07 5:38 AM | ||
Hello everyone, I'm working on the LORA pingpong example, and in the pingpong_process code, where I...
| 2023-07-28 1:14 PM | ||
Hello, When I execute StartEcc() in a code without TrustZone enabled, it sets the ECCE & ALE bits ...
| 2023-07-27 11:52 PM | ||
Need help. I have a problem with the implementation of the tcp-client. I use STM32H7, FreeRTOS, LW...
| 2023-07-19 6:38 AM | ||
Hello
I am looking for information about the available Wi-Fi modules that I can use for an IoT ap...
| 2023-07-19 1:24 AM | ||
Hello, I'm working on a project related to SPWM modulation for inverters, I´m using two timers, TIM...
| 2023-07-18 8:13 AM | ||
Hi I want to communicate azure iot hub using cellular modem. I have bg95 mini pcie evm kit, need ...
| 2023-07-16 11:32 PM | ||
Hi, I'm doing a project which sends CAN data from B-G431B-ESC1 board to sth else(NI cRio). Just to...
| 2023-07-12 11:50 PM | ||
I try to interface the SX1262MB2CAS Lora module with STM32F103 board. I need to support software...
| 2023-07-10 9:57 PM | ||
Hi Community, I am using a cross-compiled library with STM32CubeIDE which uses regcomp, regexec, an...
| 2023-07-04 5:14 AM | ||
Hi, I tried to do the Cellular:Cellular_X-CUBE-CELLULAR_How_To Wiki. But when I send the atcmd AT+...
| 2023-06-30 2:16 AM | ||
Hello, I am new to STM, I wanted to know, How can be FOTA implemented for STM32F446ZET6?are there ...
| 2023-06-27 11:32 PM | ||
Hello everyone,
I am developing an application using I-CUBE-LRWAN1 and a set of my own sensors to...
| 2023-06-26 11:54 AM | ||
My project requires the use of Threadx Modules. Using the TX_MPU example as a guide I have successf...
| 2023-06-26 3:40 AM | ||
Hi, I have the TFM example running on my board. I'm now trying to write my own non-secured appli...
| 2023-06-25 10:20 AM | ||
Hi, I am very new to STM32. Also new to programming, IDE etc. I am trying to make an OLED print out...
| 2023-06-22 4:54 AM | ||
I would like to try a PPP connection with P-L496G-CELL02 + BG96 board with X-CUBE-CELLULAR v7.0.0. ...
| 2023-06-22 4:15 AM | ||
I was under the impression the adc handler would by default generate a flag to exit the sleep mode....
| 2023-06-21 8:39 PM |