| Subject | Author | Posted | |
|---|---|---|---|
|
I am using I2S (SAI) on the STM32L433 nucleo board and using the internal MSI RC as the clock sourc...
| 2025-12-17 12:41 PM | ||
|
Hello, I have application which go to STOP2 mode once no LPUART/Modbus communication (Running at 3...
| 2025-12-16 10:20 PM | ||
|
Hello, I'm working on finding the smallest possible power solution for the STM32N6. The refer...
| 2025-10-14 5:44 AM | ||
|
Post edited by ST moderator to be inline with the community rules especially with the code sharing....
| 2025-09-17 10:02 AM | ||
|
I connected the nucleo board with the cpu using port CN6 using USB-C cable with BOOT0 and BOOT1 set...
| 2025-09-08 12:28 AM | ||
|
Hello, When using stop mode 3 with the stm32u5a9j chip, I noticed a unexpected behaviour when exit...
| 2025-08-26 2:40 AM | ||
|
Dear ST Community, I am using the STM32H573's SDMMC interface to communicate with a soft eMMC devi...
| 2025-08-07 7:47 AM | ||
|
Hello,
we use STM32F413RGT6 as slave board communicate through rs485 bus. In application, we driv...
| 2025-07-28 7:27 AM | ||
|
Moved from this thread.
What is the maximum amount of time required after bringing nRST high for ...
| 2025-07-09 8:17 AM | ||
|
I'm writing a small HAL of my own for the STM32F1 and I noticed that sometimes the DMA would read i...
| 2025-06-09 6:18 PM | ||
|
Hello. I work on a project (the microcontroller is STM32H733VGT6) where VBAT mode is used. When th...
| 2025-06-03 3:36 AM | ||
|
I'm working on a project which uses DMA to pull data from an external chip controlled by the FMC in...
| 2025-05-29 1:25 PM | ||
|
Hello, I am using STM32F030C8T6 to implement Modbus RTU protocol which uses UART and RS485 as phys...
| 2025-05-23 1:07 PM | ||
|
Board: NUCLEO-H723ZG MCU: STM32H723ZG (applies to others as well) Reference manual: RM0468 Rev. 3...
| 2025-05-21 12:56 AM | ||
|
Hi, I have an STM32F407-DISC1 connected to an Raspberry PI via I2S. The clock frequency is about 3M...
| 2025-05-20 1:42 AM | ||
|
Hi I'm planning to make a digital mixer that takes 4 analog audio input channels (2x stereo), proc...
| 2025-04-29 5:37 AM | ||
|
I'm working on recording audio synchronously using multiple I2S microphones connected to different ...
| 2025-04-23 3:57 AM | ||
|
Hello, I am working on a simple project at STM32L476 NUCLEO which includes ADC1 + TIM6 + DMA1. No ...
| 2025-04-09 1:25 PM | ||
|
Moved from Feedback Forum.
The Feedback Forum is not for product questions.
Hello ev...
| 2025-04-03 1:47 AM | ||
|
Hello, I am working with the STM32H503CBT6 and using the I3C Transmit_IT in Controller mode for co...
| 2025-03-28 12:46 AM |