| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, Anyone can help with resources (videos, Documents), to understand how to calculate time dela...
| 2025-03-10 9:40 PM | ||
|
I'm trying to use a STM32 Nucleo-L476RG to get audio from a PDM MEMs Microphone (Infineon IM66D120A...
| 2025-03-10 12:02 PM | ||
|
Hello, I am trying to write to the option byte area of an stm32u5g9vjt6q using the built in bootloa...
| 2025-02-23 12:53 PM | ||
|
Hello, I have a NUCLEO U545 - REQ and i have a Queue in which i read the incoming values from ...
| 2025-02-21 2:25 AM | ||
|
Can anyone comment on the prologue and epilogue of following CM7 code, particularly the content of ...
| 2025-02-03 5:37 AM | ||
|
Howdy, I am currently working with a STM32U575 and currently having a problem with the ADF. I am t...
| 2025-01-27 9:29 AM | ||
|
Hi everyone, I’m working on a custom board design using an STM32H753AII6 in the UFBGA169 package. ...
| 2025-01-23 2:03 AM | ||
|
Hello, I am considering the STM32H7 for a new project I'm working on. I'd like to configure the M...
| 2025-01-16 2:39 PM | ||
|
I am trying LTDC color keying application. LTDC uses HSI as clock source. I want to make all system...
| 2024-12-30 9:06 AM | ||
|
Hello everyone, why is it that the ITM output does not display when the IDE jumps from boot to Appl...
| 2024-12-30 12:52 AM | ||
|
Hello everyone I need to implement a protocol for an external ADC. An SPI read with 22 bits should...
| 2024-12-18 2:05 AM | ||
|
Dear community, It is now public and available at distributors : https://www.st.com/stm32n6
| 2024-12-17 12:48 AM | ||
|
I am trying to read the data interpreted in a SIF signal using a Nucleo-F072RB. There are three p...
| 2024-12-11 8:02 PM | ||
|
This code, partially generated by Copilot, does only print "=" At the same time, I do see that the...
| 2024-12-10 10:09 AM | ||
|
In STM32H735IGT mcu I have initialized ADC1 and ADC3 in DMA method, also FreeRTOS is initialized. B...
| 2024-12-10 3:17 AM | ||
|
I am experiencing an issue with the STM32 microcontroller used in a Battery Management System (BMS)...
| 2024-12-09 9:34 PM | ||
|
Hello, I use STM32F407G-DISC1 with Digilent PMOD I2S2. I have FIR filter project and after i enabl...
| 2024-12-09 10:07 AM | ||
|
Hello folks!
One of my devices happened to have a some kind of flash corruption, enough that an E...
| 2024-12-05 12:10 AM | ||
|
I am useing ADC with STM32H743ZIT6 device.when i debugging,i find that the device can't read DBGMCU...
| 2024-11-29 7:44 AM | ||
|
Hi, I am trying to do synchronous DAC and ADC sampling using timers on the STM32H747. A simplifie...
| 2024-11-29 6:53 AM |