| Subject | Author | Posted | |
|---|---|---|---|
|
Hi! Please guide me how to implement hardware flow control for inter-communication between two boa...
| 2024-05-23 3:57 AM | ||
|
I had EMI problems interfacing with my 4.0" ILI9488 v1.1 display over SPI. Having a long cable (abo...
| 2024-05-22 9:24 AM | ||
|
Hi all, I am trying to program some data to an external NAND flash chip(connected by FMC) by STM32...
| 2024-05-22 3:00 AM | ||
|
I am trying to read NFC tags using the NFC03A1 NFC Module and the NUCLEO F439ZI, but I am not able ...
| 2024-05-22 2:28 AM | ||
|
Hello, i am trying to configure the STUSB4500 on a Eval-SCs001v1 with a F446RE Nucleo board using ...
| 2024-05-21 6:33 AM | ||
|
Hello, We're currently facing a weird problem with our project and FreeRTOS. I've asked in the Fre...
| 2024-05-21 5:20 AM | ||
|
#include "main.h"
/* Private includes ---------------------------------------------------------...
| 2024-05-20 6:44 AM | ||
|
I would like to use the ADC3 of the STM32H7 series chip to realize that the voltage is collected on...
| 2024-05-20 4:01 AM | ||
|
Hi All: We have a project to receive pdm microphone based on the STM32L476RG-Nucleo board. We hop...
| 2024-05-20 3:55 AM | ||
|
Hello! I am following this tutorial to setup FreeRTOS on STM32F446ZE using MicroROS on Raspberry Pi...
| 2024-05-19 8:35 PM | ||
|
Hi I am designing PCB with the MCU above. I do not have any devboard for now with G0 to check what...
| 2024-05-17 3:05 AM | ||
|
Hi, I have an application code(Call it as Code-1). I able to dump it into my custom STM32H735...
| 2024-05-17 2:18 AM | ||
|
Hi. I'm using Keil5. ADC encountered an error in my program(from function HAL_ADC_PollForConversio...
| 2024-05-17 12:52 AM | ||
|
I brought the sinewave with 120mVpp amplitude as positive input to STM32G431K8 onboard comparator (...
| 2024-05-16 4:15 AM | ||
|
I am working with the NAND Flash 5 Click module, the STMOD+, and the STM32H750B Disco board. My goa...
| 2024-05-15 1:51 AM | ||
|
I found an Oscilloscope project (https://www.youtube.com/watch?v=sSbzYbYM4iM) but I want to make th...
| 2024-05-14 11:59 PM | ||
|
We are using STM32L053R8. What is the best method (Clock and Low power modes) to achieve lowest p...
| 2024-05-13 10:10 PM | ||
|
Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelect...
| 2024-05-11 4:00 AM | ||
|
I trying to program a nucleo-144 L496GZ-P board which has been split from the st-link. I've connect...
| 2024-05-10 8:19 AM | ||
|
started using STM32H573 recently, having issues with Flash Edata when reading data from EData area,...
| 2024-05-09 9:02 PM |