Hello, I am developing a firmware for a host device to flash STM8S via UART. My issue is when I send a write command, STM8 didn't response anything. - Host sends write command: 0x31 0xCE, STM8 res...
Hello community, I'm looking for materials to learn STM8S programming. I searched on the internet but I couldn't find anything. Can you recommend me any documents or links to learn, please? Thank ...
I'm trying to get my STM8AF5288 to read CAN from a TJA1050. I had it reading perfectly. 1Mbps @ 16Mhz. Using time_seg1 of 8, tim_seg2 of 7, prescale of 1. SJW1. The sending u...
I am trying to program the STM8S001J3 microcontroller, on a custom board. I am using ST Visual Programmer tool for flashing the program but I’m running into the following error continuously. I h...
I download firmware in s19 format via STVP program. I would like to know how to check the checksum of firmware via STVP_Cmdline. How can I check it through the command?
Hello STM community. I have in my possesion an ST microcontroller with the following information printed on it: 72F521AR5T 99021 V5 MYS 99 and 3 other digits in the end which I am not...
Hello, STM8S208RB microcontroller. Pins PA4 and PA5 do not work in push-pull mode. Why? I haven't tried it in other modes. It's not a microcontroller issue because I tested it on two different ...
Hello. I am trying to modify my s19 file which is generated for stm8 using stvd and cosmic c compiler. Consider an S19 file which starts from 0x4000 address [EEPROM starting address] The fi...
I would like to know where the configuration set in STVP is stored. I'd like to set the configuration automatically, but I don't know where the default storage address is.