I have set up a project in STM32CubeMX. I have setup both I2S1 for Receiving and I2S2 for Transmiting with DMA. After the normal initalization i start receiving from the DMA: if (H...
The following are some questions related to the absolute maximum ratings of the TSV912IQ2T which are not clear from the datasheet. Can the voltage on the input pins (2,3,5 and 6) swing to ...
I am currently working on repairing a Taramps MD3000.1 car amplifier. There is an ST chip with the following markings: 319 MZLBD38 or it could be MZLB038. I'm not sure what it is and am having quit...
Hello, I have a guitar amp Laney LA65C where the output amp is faulty, it consists of a TDA7294 IC, I put in a new TDA7294 but it exploded as soon as the power was turned on. I checked the input volt...
Hello, I am attempting to identify a component from a switch mode power supply out of a audio preamp. I am 90% confident it is a zener diode, but after that I am at a loss. Marking...
Hi, I hope finding an answer this is my first time asking you.
So, I'm trying to build a CLASS_D AMPLIFIER with codec (STA309A).
This codec has 8 input channels for serial AUDIO and I want ...
Need to replace this. I'm assuming the one on the left is toast just from a visual inspection.
Can someone tell me which specific version I need to get? I'm not sure if the "EZ605" designator means...