2025-01-28 03:36 PM
Why the "wireless MCU" category does not have all the tags as the "normal" STM32s MCUs?
If the post is about SPI on STM32WB, I cannot tag it both STM32WB and SPI. All tags for SPI, I2C and so on are available only in the normal MCU category.
2025-02-03 08:14 AM
Hello @Pavel A.,
Thanks for brining that up. Let me review this proposal with a respective team and I will get back.
Greetings,
Lina
2025-02-03 08:22 AM
Also nothing for:
2025-02-06 03:22 AM
The 'STM32 Wireless' category also lacks tags for ST boards
2025-02-11 06:51 AM
Usually, posts in the 'STM32 MCUs Boards and hardware tools' category are about a specific interface or function - Timers, UART, SPI, I2C, etc - but there are no tags for these.
The tags should include all those in the 'STM32 MCUs Products' section.
Similarly in the 'STM32 MCUs Wireless' section; especially as anything mentioning a wireless chip seems to get moved there - whether or not the post has anything to do with the wireless part
2025-02-14 09:20 AM
Hello @Pavel A. , @Andrew Neil,
We updated the label list in the board: STM32 MCUs Wireless - STMicroelectronics Community
Check it out and let us what you think.
Thanks,
Lina