2024-09-14 5:55 AM
Hello,
st.com on my system does no longer show the "three bars" menu to access e.g. "products. Hava a look at appended screenshot.
2024-09-16 6:09 AM
Hi @Uwe Bonnes,
Thanks for reporting this issue.
Looking at the post from @TJM https://community.st.com/t5/feedback-forum/st-com-website/td-p/720011
it could be an issue related to Firefox on Linux. I've forwarded this information to the respective team and will get back to you once I have more feedback.
Best regards,
Laurids
2024-09-16 7:46 AM
Good morning.
It does not appear to be a Firefox issue but maybe a Linux issue. Same thing happens with Chrome on Linux, the main panel containing numerous changing screen appears to lock out some functions including the icon that allows the login panel to present itself. This happens most of the time. An animated icon that indicates something is loading appears at the top middle of the panel and never stops. This morning the display panels are different but the issue remains. My expectation is that I should be able to select the login icon and go directly to the username/password panel at any time, but this does not happen.
Thanks,
TJM
2024-09-17 3:03 AM
I now have the endless waiting icon too.
2024-09-17 11:21 AM
This condition is extremely annoying. I can't log in. I've used a couple of links from the webinar today and while I can get to the page, I can't do anything else because the 'wait' icon transfers from page to page. This condition make it not possible to log in or to download some files from st.com that are used in the webinar.
TJM
2024-09-20 2:26 AM
Situation changed. On web page startup, still no 3 bar menu. After scrolling the page and going back to top, the menu row including the 3 bars picture appears.
2024-09-20 2:38 PM
The menu also appears without any scrolling but waiting until the first movie changed.