cancel
Showing results for 
Search instead for 
Did you mean: 

Which software do I need to install to start with STM32N6570-DK?

Anhem
Associate III

I am a newbie with STM32N6570-DK.

My target is to deploy AI model on this board. Which software do I need to install to start with STM32N6570-DK? I means that all softwares.

Thank you.

19 REPLIES 19

Hi @Julian E. 

Here is my config file

Concerning the graphic card, did you get an error ? the code should use a GPU if it finds one, but should still works even if you don't have one.

Yes, I think so and I commented out source code that check GPU

@hydra.main(version_base=None, config_path="", config_name="user_config") def main(cfg: DictConfig) -> None: """ Main entry point of the script. Args: cfg: Configuration dictionary. Returns: None """ # # Configure the GPU (the 'general' section may be missing) # if "general" in cfg and cfg.general: # # Set upper limit on usable GPU memory # if "gpu_memory_limit" in cfg.general and cfg.general.gpu_memory_limit: # set_gpu_memory_limit(cfg.general.gpu_memory_limit) # else: # print("[WARNING] The usable GPU memory is unlimited.\n" # "Please consider setting the 'gpu_memory_limit' attribute " # "in the 'general' section of your configuration file.")
Anhem
Associate III

@Julian E. 

Here is my user_config.yaml. I keep it the same as initial. I see stedgeAI and IDE paths. Do I need to change these paths?

I also see there is some places for board STM32H7. Do I need to changed these places?

general: project_name: COCO_2017_person_Demo model_type: st_yolo_lc_v1 #choices=[st_ssd_mobilenet_v1, ssd_mobilenet_v2_fpnlite, tiny_yolo_v2, st_yolo_lc_v1, # st_yolo_x, yolo_v8, yolo_v5u] model_path: logs_dir: logs saved_models_dir: saved_models gpu_memory_limit: 16 num_threads_tflite: 4 global_seed: 127 operation_mode: chain_tqeb #choices=['training' , 'evaluation', 'deployment', 'quantization', 'benchmarking', # 'chain_tqeb','chain_tqe','chain_eqe','chain_qb','chain_eqeb','chain_qd '] dataset: name: COCO_2017_person class_names: [ person ] training_path: /dataset/coco_person_2017_tfs/train validation_path: validation_split: 0.1 test_path: /dataset/coco_person_2017_tfs/val quantization_path: /dataset/coco_person_2017_tfs/val quantization_split: 0.01 preprocessing: rescaling: { scale: 1/127.5, offset: -1 } resizing: aspect_ratio: fit interpolation: nearest color_mode: rgb data_augmentation: ########## For tiny_yolo_v2 and st_yolo_lc_v1 only ########### random_periodic_resizing: period: 10 image_sizes: [(192, 192), (224, 224), (256, 256), (288, 288), (320, 320), (352, 352), (384, 384), (416, 416), (448, 448), (480, 480), (512, 512), (544, 544), (576, 576), (608, 608)] random_flip: mode: horizontal random_crop: crop_center_x: (0.25, 0.75) crop_center_y: (0.25, 0.75) crop_width: (0.5, 0.9) crop_height: (0.5, 0.9) change_rate: 0.9 random_contrast: factor: 0.4 random_brightness: factor: 0.3 training: model: # alpha: 0.35 input_shape: (192, 192, 3) # pretrained_weights: imagenet dropout: batch_size: 64 epochs: 4 optimizer: Adam: learning_rate: 0.005 callbacks: ReduceLROnPlateau: monitor: val_map patience: 10 factor: 0.25 ModelCheckpoint: monitor: val_map EarlyStopping: monitor: val_map patience: 20 postprocessing: confidence_thresh: 0.001 NMS_thresh: 0.5 IoU_eval_thresh: 0.4 plot_metrics: False # Plot precision versus recall curves. Default is False. max_detection_boxes: 100 quantization: quantizer: TFlite_converter quantization_type: PTQ quantization_input_type: uint8 quantization_output_type: float granularity: per_channel #per_tensor optimize: False #can be True if per_tensor export_dir: quantized_models benchmarking: board: STM32H747I-DISCO tools: stedgeai: version: 10.0.0 optimization: balanced on_cloud: True path_to_stedgeai: C:/Users/<XXXXX>/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/<*.*.*>/Utilities/windows/stedgeai.exe path_to_cubeIDE: C:/ST/STM32CubeIDE_<*.*.*>/STM32CubeIDE/stm32cubeide.exe deployment: c_project_path: ../../application_code/object_detection/STM32H7/ IDE: GCC verbosity: 1 hardware_setup: serie: STM32H7 board: STM32H747I-DISCO mlflow: uri: ./experiments_outputs/mlruns hydra: run: dir: ./experiments_outputs/${now:%Y_%m_%d_%H_%M_%S}
View more

 

When you run the command:

python stm32ai_main.py

 it uses by default the user_config.py

 

If you want to use the one you sent me in the zip you should run:

python stm32ai_main --config-name YOUR_YAML.yaml

 

You do indeed need to edit the ST Edge AI and CubeIDE paths.

(which you did in your yaml in the zip, but not in the user_config.yaml that is called if you did not specify the config-name)

 

In your error I see permission denied, so you may have to edit the permission with chmod of your stedgeai folder.

 

Let me know if it works.

Also try to revert the python file for the GPU to its original state.

 

Julian

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Julian E. 

After editing permission with

sudo chmod 777 -R /opt/ST/STEdgeAI/ sudo chmod 777 -R /opt/ST/STEdgeAI/* python3 stm32ai_main.py --config-path ./config_file_examples/ --config-name deployment_n6_ssd_mobilenet_v2_fpnlite_config.yaml

But the process took too much time and it stopped to at the point. You can see in the atttached message. I waited 30 minutes, but it did not do anything as before changing permission. My board has 2 LEDs (red and orange). It seems that I need to use USB-C to USB-C (not USB-A to USB to make sure enough power. Anyway, which cable should I use: data cable or charge cable same as for mobile phone charging?), but this is different problem.

How I can fix this issue with deployment and permission? I am afraid that I need to reinstall STEdgeAI because currently it does not run after changing permission. Thank you.

 

(stm_32)  /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src î‚° python3 stm32ai_main.py --config-path ./config_file_examples/ --config-name deployment_n6_ssd_mobilenet_v2_fpnlite_config.yaml                   

2025-03-24 09:14:14.630486: W tensorflow/stream_executor/platform/default/dso_loader.cc:64] Could not load dynamic library 'libcudart.so.11.0'; dlerror: libcudart.so.11.0: cannot open shared object file: No such file or directory
2025-03-24 09:14:14.630502: I tensorflow/stream_executor/cuda/cudart_stub.cc:29] Ignore above cudart dlerror if you do not have a GPU set up on your machine.
[INFO] : Running `deployment` operation mode
[INFO] : ClearML config check
[INFO] : The random seed for this simulation is 123
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
[INFO] : Generating C header file for Getting Started...
[INFO] : This TFLITE model doesnt contain a post-processing layer
loading model.. model_path="/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite"
loading conf file.. "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
[INFO] : Selected board :  "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
[INFO] : Compiling the model and generating optimized C code + Lib/Inc files:  /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite
setting STM.AI tools.. root_dir="", req_version=""
 Cube AI Path: "/opt/ST/STEdgeAI/2.0/Utilities/linux/stedgeai".
[INFO] : Offline CubeAI used; Selected tools:  10.0.0 (x-cube-ai pack)
loading conf file.. "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None"
"n6 release" configuration is used
compiling... "ssd_mobilenet_v2_fpnlite_035_192_int8_tflite" session
 model_path  : ['/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite']
 tools       : 10.0.0 (x-cube-ai pack)
 target      : "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6)
 options     : --st-neural-art default@/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/user_neuralart.json --input-data-type uint8 --inputs-ch-position chlast

 

Hello @Anhem,

 

First, concerning the cable, you need a data cable.

Also, make sure to connect it to the port where it says st link v3. (same side of the boot pins).

 

Then concerning the fact that it blocks, next time, can you try to press ENTER when it blocks. I believe that sometime I have to do it.

 

I think we can check if the issue comes from ST Edge AI Core or Model Zoo by manually using ST Edge AI Core. To do so, please try the following:

  1. Go to your st edge ai folder: 
    /opt/ST/STEdgeAI/2.0/Utilities/linux/stedgea
  2. Then copy your model in this folder (either a .h5, .onnx or .tflite)
  3. Open a terminal and run the command:
    ./stedgeai generate --model YOUR_MODEL --target stm32n6 --st-neural-art​

(I don't use linux, so the first part of the command is maybe wrong, but the options are good)

Let it run and if it run as it should, you should have a message saying it is complete.

If it works, we at least know that ST Edge AI core is working.

 

In the meantime, I will test the exact model that you use. I don't think it comes from that, but we never know.

 

Have a good day,

Julian

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Julian E. 

Thank you for your response.

First, concerning the cable, you need a data cable. Yes, I will use data cable usbC to usbC.

Also, make sure to connect it to the port where it says st link v3. (same side of the boot pins). Yes, it is default on the board, in JP2, STLK.  I attached the image below 

Then concerning the fact that it blocks, next time, can you try to press ENTER when it blocks. I believe that sometime I have to do it.  I tried press Enter when it is running, but it did not solve the problem. But when I tried Enter twice and wait, it seems that it can building and flashing, but I got error.

(stm_32) /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src î‚° python3 stm32ai_main.py --config-path ./config_file_examples/ --config-name deployment_n6_ssd_mobilenet_v2_fpnlite_config.yaml 2025-03-25 11:11:00.143876: W tensorflow/stream_executor/platform/default/dso_loader.cc:64] Could not load dynamic library 'libcudart.so.11.0'; dlerror: libcudart.so.11.0: cannot open shared object file: No such file or directory 2025-03-25 11:11:00.143895: I tensorflow/stream_executor/cuda/cudart_stub.cc:29] Ignore above cudart dlerror if you do not have a GPU set up on your machine. [INFO] : Running `deployment` operation mode [INFO] : ClearML config check [INFO] : The random seed for this simulation is 123 INFO: Created TensorFlow Lite XNNPACK delegate for CPU. [INFO] : Generating C header file for Getting Started... [INFO] : This TFLITE model doesnt contain a post-processing layer loading model.. model_path="/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite" loading conf file.. "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None" "n6 release" configuration is used [INFO] : Selected board : "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6) [INFO] : Compiling the model and generating optimized C code + Lib/Inc files: /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite setting STM.AI tools.. root_dir="", req_version="" Cube AI Path: "/opt/ST/STEdgeAI/2.0/Utilities/linux/stedgeai". [INFO] : Offline CubeAI used; Selected tools: 10.0.0 (x-cube-ai pack) loading conf file.. "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/stmaic_STM32N6570-DK.conf" config="None" "n6 release" configuration is used compiling... "ssd_mobilenet_v2_fpnlite_035_192_int8_tflite" session model_path : ['/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/stm32ai-modelzoo/object_detection/ssd_mobilenet_v2_fpnlite/ST_pretrainedmodel_public_dataset/coco_2017_person/ssd_mobilenet_v2_fpnlite_035_192/ssd_mobilenet_v2_fpnlite_035_192_int8.tflite'] tools : 10.0.0 (x-cube-ai pack) target : "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6) options : --st-neural-art default@/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/user_neuralart.json --input-data-type uint8 --inputs-ch-position chlast "series" value is not coherent.. stm32n6 != stm32n6npu results -> RAM=621,048 IO=110,592:153,800 WEIGHTS=1,618,465 MACC=0 RT_RAM=1,773 RT_FLASH=632,783 LATENCY=0.000 [INFO] : Optimized C code + Lib/Inc files generation done. [INFO] : Building the STM32 c-project.. deploying the c-project.. "STM32N6570-DK Getting Started Object Detection (STM32CubeIDE)" (stm32_cube_ide/n6 release/stm32n6) updating.. n6 release -> s:copying file.. "network.c" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/network.c -> s:copying file.. "network_ecblobs.h" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/network_ecblobs.h -> s:copying file.. "network_atonbuf.xSPI2.raw" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Model/network_atonbuf.xSPI2.raw -> s:removing dir.. /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Lib/GCC/ARMCortexM55 -> s:copying dir.. "ARMCortexM55" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Lib/GCC/ARMCortexM55 -> s:removing dir.. /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Inc -> s:copying dir.. "Inc" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Inc -> s:removing dir.. /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Npu/ll_aton -> s:copying dir.. "ll_aton" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Middlewares/AI_Runtime/Npu/ll_aton -> u:copying file.. "app_config.h" to /media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/Inc/app_config.h -> updating cproject file "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/application_code/object_detection/STM32N6/STM32CubeIDE" with "NetworkRuntime1000_CM55_GCC.a" building.. n6 release flashing.. n6 release STM32N6570-DK Error executing job with overrides: [] Traceback (most recent call last): File "/home/anhem/miniconda3/envs/stm_32/lib/python3.10/site-packages/clearml/binding/hydra_bind.py", line 230, in _patched_task_function return task_function(a_config, *a_args, **a_kwargs) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/stm32ai_main.py", line 228, in main process_mode(cfg) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/stm32ai_main.py", line 102, in process_mode deploy(cfg) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../deployment/deploy.py", line 111, in deploy stm32ai_deploy_stm32n6(target=board, stlink_serial_number=stlink_serial_number, stm32ai_version=stm32ai_version, c_project_path=c_project_path, File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/deployment/common_deploy.py", line 528, in stm32ai_deploy_stm32n6 stmaic.build(session, user_files=user_files, serial_number=stlink_serial_number) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/build.py", line 513, in cmd_build _cube_ide_builder(cube_ide_exe[0], session, used_conf, File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/build.py", line 470, in _cube_ide_builder _programm_dev_board(conf, session.series, serial_number=serial_number) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/build.py", line 231, in _programm_dev_board st_links, _ = get_stm32_board_interfaces(series) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/stm32_tools.py", line 329, in get_stm32_board_interfaces st_links[idx] = _stm32_get_info(app[0], serial_number=st_link['sn'], series=series) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/stm32_tools.py", line 309, in _stm32_get_info run_shell_cmd(cmd_line, logger=cur_logger, parser=parser, assert_on_error=True) File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/utils.py", line 312, in run_shell_cmd raise excep_ File "/media/anhem/mnt/STM32N6570DK_dev/stm32ai-modelzoo-services-1dc52d8ef939fb7875c6e00e7a6f6311f07c5cb1/object_detection/src/../../common/stm32ai_local/utils.py", line 305, in run_shell_cmd raise RuntimeError('invalid command ' + '\"{}\"'.format(str_args)) RuntimeError: invalid command "STM32_Programmer_CLI --connect port=SWD mode=HOTPLUG -hardRst sn=0025001F3333511831363730" Set the environment variable HYDRA_FULL_ERROR=1 for a complete stack trace.
View more

It seems that it is error with STM32_Programmer_CLI. I tried to add STM32_Programmer_CLI to PATH of Ubuntu and run this command

STM32_Programmer_CLI --connect port=SWD mode=HOTPLUG sn=0025001F3333511831363730

And I got this output

------------------------------------------------------------------- STM32CubeProgrammer v2.19.0 ------------------------------------------------------------------- ST-LINK SN : 0025001F3333511831363730 ST-LINK FW : V3J15M6 Board : STM32N6570-DK Voltage : 3,29V Error: Unable to get core ID Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication 2nd connect tentative with frequency (8MHz) ST-LINK SN : 0025001F3333511831363730 ST-LINK FW : V3J15M6 Board : STM32N6570-DK Voltage : 3,29V Error: Unable to get core ID Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

It seem that, the board is detected but STM32 core is not found. How can I fix it? Current my setting: BOOT0 - Right, BOOT1 - Left, use Jumper STLINK, connect board with PC via USB-A to USB-C. How can I fix this issue?

 

I think we can check if the issue comes from ST Edge AI Core or Model Zoo by manually using ST Edge AI Core. To do so, please try the following:

  1. Go to your st edge ai folder: 
    /opt/ST/STEdgeAI/2.0/Utilities/linux/stedgea
  2. Then copy your model in this folder (either a .h5, .onnx or .tflite)
  3. Open a terminal and run the command:
     
    ./stedgeai generate --model YOUR_MODEL --target stm32n6 --st-neural-art​

(I don't use linux, so the first part of the command is maybe wrong, but the options are good)

Let it run and if it run as it should, you should have a message saying it is complete.

If it works, we at least know that ST Edge AI core is working.

Yes, I check on my side, ST Edge AI works well. Here is output and some generated files. Please see the attached images and log file

 

In the meantime, I will test the exact model that you use. I don't think it comes from that, but we never know.  Yes, thank you so much. Now I am stucked here and I could not revert initial permession of STEdgeai.

 

I am waiting good news from you. Thank you so much.

 

Julian E.
ST Employee

Hello @Anhem,

 

Please set both boot pin to the right. This should solve the issue.

Also, please try to only use USB-C to USB-C data cable. When the application will run, you will encounter an issue because of the insufficient voltage.

 

Have a good day,

Julian 

 

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Julian E. 

Please set both boot pin to the right. This should solve the issue.

https://github.com/STMicroelectronics/stm32ai-modelzoo-services/blob/main/object_detection/deployment/README_STM32N6.md#table-of-contents in this guide in deployment part. Step 3.3 said that BOOT0 - RIGHT and after running commands

cd ../src/ python stm32ai_main.py --config-path ./config_file_examples/ --config-name deployment_n6_ssd_mobilenet_v2_fpnlite_config.yaml

both pins are set to the LEFT. 

So I will try as your comment. Firstly I will set both pins to RIGHT and after running Python script I wall set both pins to LEFT to run inference.

Also, please try to only use USB-C to USB-C data cable. When the application will run, you will encounter an issue because of the insufficient voltage.

Yes, I understood

 

Thank you so much. I could successfully run tfllite model from Model zoo. You are right, we need to set both BOOT pins to the right before running Python script, after that turn them to LEFT. I also used USB-C to USB-C data cable (led LD3 is yellow-green => that's fine). Moreover, in Linux we need to solve permission issue and PATH of some STM32 components. That is from my experience that I want to share.

 

I have one more question. As my understanding, currently I am running with internal flash (user internal memory). Is that right? and How much memory I can use with this model? I want to know this value to estimate whether my AI model can be run with this settings.

 

Moreover, I know that STM32N6570-DK supports SD card. It means that we can deploy all C source code + AI model to SD and run inference for LARGER models. Is that right? If it is correct, could you please provide guide link to do this (about how to set up board to run with SD card, how to build and flash, it is better if it comes with AI model).

 

Hello @Anhem,

 

You can find the memory available and used when doing a stedgeai generate. For example:

JulianE_2-1742978429606.png

https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_getting_started.html

 

When you use external memory (other than cpu and npu ram in the image above), the performance in terms of inference time reduce drastically as it needs to gather the data from external memory before using it.

 

So yes, you can run larger model and use SD card, but it is not advised. If your use case do not need a fast inference time for any reason, it can be useful though.

 

I am not an embedded engineer, so I don't really know how to use a SD card. You can ask the MCU forum board about that. 

Regarding AI, you will for sure need to edit the memory-pool file:

JulianE_3-1742979017168.png

Memory-pool descriptor: file: $STEDGEAI_CORE_DIR/Utilities/windows/targets/stm32/resources/mpools/stm32n6.mpool.

 

When you use the st edge ai core, it looks at your memory pool file that indicate what kinds of memories are available, their start adress, size etc.

 

If you look at the default one, you will see that you have a description of the memories available that correspond to the first image I sent.

JulianE_4-1742979208247.png

 

Because our real use case tends to be focusing on fast inference time, we don't currently have any example using SD Card.

 

Have a good day,

Julian

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Julian E. 

When you use external memory (other than cpu and npu ram in the image above), the performance in terms of inference time reduce drastically as it needs to gather the data from external memory before using it.

So yes, you can run larger model and use SD card, but it is not advised. If your use case do not need a fast inference time for any reason, it can be useful though.

Yes. I understood. That is valuable information.

 

Regarding AI, you will for sure need to edit the memory-pool file.

Because our real use case tends to be focusing on fast inference time, we don't currently have any example using SD Card.

Yes, I understood that I need to set up memory address.

Thank you again for supporting me. Have a nice day.