cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 isn't detected

Fcaru
Associate II

I have a problem with STM32; when i connect my FC the STM32 it isn't detected from my pc, it doesn't appear in device manager. What is the problem? I have windows 10 a OS. I tried out to install cube programmer, zadig, but STM32 isn't detected. Thanks for the support!!

6 REPLIES 6
fauvarque.daniel
ST Employee

What board are you using ?

If you are using an ST board with an embedded ST-Link make sure you connect the board on the USB port marked ST-Link.

Also, you may download the STLink firmware upgrade to upgrade the firmware on the ST-Link https://www.st.com/en/development-tools/stsw-link007.html

and the driver https://www.st.com/en/development-tools/stsw-link009.html

Regards

Daniel


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Some Flight Controller? Be SPECIFIC, perhaps cite a web page for the specific hardware you're talking about.

Device might not be powered correctly

Device might not be in the correct mode to connect. Is there a BOOT button, are you connecting via USB?

Does ANYTHING show up in Device Manager? What?

Try a different cable

Try a different port

Avoid docking stations and hubs

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Fcaru
Associate II

Sorry, i am using a SP Racing F3 as flight controller, and on it is installed the STM32. The whole thing is to manage a x220 wizard.

I tried out to change port, usb cable, also with boot button, but when i connect it to pc in device manager, in particular in "USB devices", there isn't STM32. Thanks for the answers.I attached the manual about the FC.I tried on modeling sites but nobody can give me answers and I think it's a problem with the STM32.

fauvarque.daniel
ST Employee

According to the documentation you need an external standalone ST-Link to program and debug the embedded MCU

https://www.st.com/en/development-tools/st-link-v2.html


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Fcaru
Associate II

So i have to buy this module? Can't be solved by installing some special software?

Fcaru
Associate II

Thanks for the suggestion, is there any other help? Because other that are bought this drone haven't bought this module, this is why it seems strange to me.