2024-07-25 01:12 AM
Hi,
I have just opened my new STEVAL-PROTEUS1 evaluation kit for my project. I tried to connect it with the STBLE sensor app, but I realized that it does not appear on the Bluetooth search. Then I tried my STEVAL-STWINKT1B sensor kit, and it connected, so I assume that the issue is not related to the cable. Do you have any solution for this problem? I would appreciate it very much if you could help with this.
Solved! Go to Solution.
2024-07-25 07:53 AM
Thank you for your response. While reviewing the datasheet, I realized that the J10 jumper needed to be opened to provide power. After doing this, it was fixed. I guess I should read the datasheet more carefully 🙂
2024-07-25 07:44 AM
Hello @Batuhan35
Support from BLESensor app depends on the firmware running on the eval boards. Are you sure you've never updated the firmware? Which version of BLESensor app are you using?
There are different examples that can be flashed on both PROTEUS or STWIN board, each one exploiting specific features. Complete lists are here and here.
Best regards
Simone
2024-07-25 07:53 AM
Thank you for your response. While reviewing the datasheet, I realized that the J10 jumper needed to be opened to provide power. After doing this, it was fixed. I guess I should read the datasheet more carefully 🙂