2022-09-15 7:04 AM
Hello,
In the annex video it is mentioned that the project archive is available for the Nucleo board project with X-NUCLEO-IKA01A1, however when I download the materials archive it appears to be missing.
Could you confirm this is the case, if so would it be possible to make this project available for download also?
Many thanks,
Anthony
Solved! Go to Solution.
2022-09-16 1:04 AM
Hi Anthony,
The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).
https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8
Best regards,
Bartosz
2022-09-15 11:21 PM
Hello Anthony,
Do you mean NEAI Studio workshop repository on the googledrive ?
Best regards,
Bartosz
2022-09-16 12:47 AM
Hi Bartosz,
This may be what I am looking for, could you share the link?
Thanks,
Anthony
2022-09-16 1:04 AM
Hi Anthony,
The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).
https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8
Best regards,
Bartosz
2022-09-16 1:21 AM
Hi Bartosz,
That's great, thank you! I will study that.
Anthony