Question
Problem with LSTM from pytorch.
Hi,
I am trying to deploy a network based on LSTM created with pytorch. The model is analysed correctly but validation on Desktop gives the following error:
LOAD ERROR: exception: access violation reading 0x0000000000000004
In the MCU a hardfault raises at inference.
I noticed that the error happens because I am accessing the 'hidden_state' of the first LSTM layer to feed it to the second one.
Any ideas about why is this happening?
This is a simple version of the model that reproduces the problem:
import torch
from torch import nn
class LSTMModel(nn.Module):
def __init__(self, input_size, hidden_size, output_size):
super(LSTMModel, self).__init__()
self.lstm1 = nn.LSTM(input_size, hidden_size, batch_first=True)
self.lstm2 = nn.LSTM(hidden_size, hidden_size, batch_first=True)
self.linear = nn.Linear(hidden_size, output_size)
def forward(self, x):
out, (hidden_state, _) = self.lstm1(x)
out, _ = self.lstm2(hidden_state)
out = self.linear(out[:, -1, :])
return out
if __name__ == '__main__':
model = LSTMModel(14, 8, 14)
input_data = torch.randn(1, 1, 14)
_ = model(input_data)
output_file = 'test-model.onnx'
model.eval()
dummy_input = torch.randn(1, 1, 14)
torch.onnx.export(
model,
dummy_input,
output_file,
verbose=False)