cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-N657X0-Q: X-Cube-AI Application stuck while running quantized TFLite model

Coop23
Associate

Hi,

I'm working on a NUCLEO-N657X0-Q board with all the newest software releases. The model I've uploaded stalls on one epoch forever while debugging or running the app. I'm trying to debug the following generated inference loop (in app_x-cube-ai.c file) of the X-Cube-AI application generated with CubeMX for a TFLite model quantized to int_8 (also attempted with ONNX-converted model):

void MX_X_CUBE_AI_Process(void)
{
    /* USER CODE BEGIN 6 */
  LL_ATON_RT_RetValues_t ll_aton_rt_ret = LL_ATON_RT_DONE;
  const LL_Buffer_InfoTypeDef * ibuffersInfos = NN_Interface_Default.input_buffers_info();
  const LL_Buffer_InfoTypeDef * obuffersInfos = NN_Interface_Default.output_buffers_info();
  buffer_in = (uint8_t *)LL_Buffer_addr_start(&ibuffersInfos[0]);
  buffer_out = (uint8_t *)LL_Buffer_addr_start(&obuffersInfos[0]);
  LL_ATON_RT_RuntimeInit();
  // run 10 inferences
  for (int inferenceNb = 0; inferenceNb<10; ++inferenceNb) {
    /* ------------- */
    /* - Inference - */
    /* ------------- */
    /* Pre-process and fill the input buffer */
    //_pre_process(buffer_in);
    /* Perform the inference */
    LL_ATON_RT_Init_Network(&NN_Instance_Default);  // Initialize passed network instance object
    do {
      /* Execute first/next step */
      ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(&NN_Instance_Default);
      /* Wait for next event */
      if (ll_aton_rt_ret == LL_ATON_RT_WFE) {
        LL_ATON_OSAL_WFE();
      }
    } while (ll_aton_rt_ret != LL_ATON_RT_DONE);
    /* Post-process the output buffer */
    /* Invalidate the associated CPU cache region if requested */
    //_post_process(buffer_out);
    LL_ATON_RT_DeInit_Network(&NN_Instance_Default);
    /* -------------------- */
    /* - End of Inference - */
    /* -------------------- */
  }
  LL_ATON_RT_RuntimeDeInit();
    /* USER CODE END 6 */
}

 

The inference loop is stalling on line 26 above, where ll_aton_rt_ret never equals LL_ATON_RT_DONE to indicate the model is done with inference. When I debugged the function LL_ATON_RT_RunEpochBlock, I found that after epoch 3, the following line is never true, stopping the model from progressing any further and continuously looping back:

if ((nn_instance->exec_state.triggered_events & _wait_mask) == _wait_mask)

 

I'm guessing the problem is with LL_ATON_OSAL_WFE() which is supposed to wait until the layer is finished with a step.

 

I haven't changed any code at all yet in this application (changed several other drafts to try and get past this). I'm very confused on why I can't get the application to work since the model runs well when I use 'Validate on Desktop' and 'Validate on Target' options in CubeMX. Any help would be greatly appreciated.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Coop23 

 

Sorry for the delay. It took more time than expected.

 

You can find the article here:

Nucleo N6:  How to build an AI application from scratch on the... - STMicroelectronics Community

DK N6: How to build an AI application from scratch on the... - STMicroelectronics Community

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Julian E.
ST Employee

Hello @Coop23,

 

STM32CubeMX does not handle well the N6, so there are errors in generation, memory activation etc.

We are finalizing tutorials for the DK and Nucleo boards. It should be ready this week.

 

I noted that you need it and will update you once available.

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @Coop23 

 

Sorry for the delay. It took more time than expected.

 

You can find the article here:

Nucleo N6:  How to build an AI application from scratch on the... - STMicroelectronics Community

DK N6: How to build an AI application from scratch on the... - STMicroelectronics Community

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.