cancel
Showing results for 
Search instead for 
Did you mean: 

NanoEdge AI Studio updates

MaxC
Associate III

Dear STM,

is there a way to avoid the installation of a new version of NanoEdge AI when a new version is available ?

Or maybe to pospone the installation ?

When a new version is available I got a dialog Win like the one below, if I click on Exit then the app closes itself, if I click on Download then the application downloads the new version and it tries to install the new version. Unfortunately, based on specific company policies, I haven't the Admin priviledeges to install every new version when it becomes available.

 

MaxC_0-1728993958617.png

 

thanks

   Max

 

1 ACCEPTED SOLUTION

Accepted Solutions
Julian E.
ST Employee

Hello @MaxC ,

I would answer that sadly you cannot skip an update.

But you can try to disconnect your pc from internet and click on Download. You should be able to use NanoEdge AI Studio normally (but it is still advised to do the update)

 

The option to postpone an update is planned and will be integrated in the next version.

Because it will be added in the next version, you will not be able to skip this one, but the ones after it.

 

Have a good day,

Julian

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Julian E.
ST Employee

Hello @MaxC ,

I would answer that sadly you cannot skip an update.

But you can try to disconnect your pc from internet and click on Download. You should be able to use NanoEdge AI Studio normally (but it is still advised to do the update)

 

The option to postpone an update is planned and will be integrated in the next version.

Because it will be added in the next version, you will not be able to skip this one, but the ones after it.

 

Have a good day,

Julian

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello Julian,

thank you for the feedback.

  Max