Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Roadmap for Learning AI in Embedded Systems

Hello everyone,I’m an embedded software engineer currently working with STM32 microcontrollers, and I am very interested in understanding how AI is being integrated into embedded systems.I would like to know:What are the common approaches or framewor...

Rajes by Associate
  • 1176 Views
  • 2 replies
  • 1 kudos

Resolved! Deploying neural networks.Tflite on N657X0 Nucleo

Hi, I have been trying to deploy simple neural networks.tflite on the STM32 N657X0 board, by applying the XCUBEAI, running under NPU.While, I have not made it work yet. If anyone has such project or docs to share, It would be highly appreciated. Best...

HANITALY by Associate III
  • 717 Views
  • 3 replies
  • 3 kudos

Debug issue on STM32N6570-DK: Target not responding

 Hello,I am working with the STM32N6570-DK board and running the STM32N6-GettingStarted-ObjectDetection example. When I debug the program in CubeIDE (The MCU runs in Dev mode), I encounter the following issue:In the main loop, when the function LL_AT...

Optimizing memory consumption of models with STEdgeAI-Core

Dear all,I'm in the process of converting a convolutional neural network from quantized ONNX format to run on the STM32N6 Neural ART NPU, using the STEdgeAI tool. I do not have access to external RAM on our custom hardware, so everything has to fit i...

asdfasdf by Associate III
  • 475 Views
  • 1 replies
  • 0 kudos

Resolved! Error reported when trying to anaylze model

Hi! My situation is the same as post provided here: https://community.st.com/t5/edge-ai/getting-error-quot-analyze-fail-on-the-ai-model-quot/td-p/55309Is there any solution to this problem? Also, I am using the STM32F407G-DISC1 board with a Mac with ...

Resolved! Example for the STM32N6570-DK kit fails

Dear all,I have the STM32N6570-DK ,MB1860B  version . I'm trying to follow the procedure to flash the .bin files. The programming seems ok, but when I reboot the kit, there's no application... the screen is inactive. However, I can successfully flash...

Issue with the STM32N6570-DK knowledge base article

Hi @Julian E.    While following along the tutorial: How to build an AI application from scratch on the... - STMicroelectronics Community after selecting the x-cube-ai package a described, I see that the default is enabled for fsbl and I cannot chang...

SM19X_0-1755334734819.png SM19X_1-1755334828632.png SM19X_0-1755425159793.png SM19X_0-1755425410157.png
SM19X by Associate II
  • 1378 Views
  • 10 replies
  • 1 kudos

Resolved! Recommended platforms for Audio Event detection model zoo

In the STM32 model zoo github repo, only the STM32U5 is listed as a recommended platform for the Audio Event Detection models.I'm trying to work out why the STM32N6 (and other devices) are not listed.Is it because it has not yet been tested, or is th...

louisfh by Associate
  • 552 Views
  • 3 replies
  • 0 kudos