2024-08-29 10:05 PM
Hi All,
I’m trying to hunt down the best board for my new project. Basically I need the following functionality either on the board or via add-on boards. I can see a few possibilities but I haven’t had much experience so I thought it best to ask. Thankyou!
Requirements
Not a requirement but would be great
2024-10-08 03:05 AM - edited 2024-10-09 12:02 AM
Hello @mzvitzf ,
Sorry for the late reply.
Seeing your requirements, all I can think of is the u85 IoT: B-U585I-IOT02A - Discovery kit for IoT node with STM32U5 series - STMicroelectronics
But it has not ethernet port and not the right audio codex.
This board is what we use for all AI audio event sound detection use case, so it is compatible with model zoo deployment for audio event detection use case as well. You can take a look here: https://github.com/STMicroelectronics/stm32ai-modelzoo/tree/main/audio_event_detection/deployment
You can also take a look at the STM32U575I-EV but it is somewhat pricy and does not have a RJ45, a audio out and is not low power...
Have a good day,
Julian