cancel
Showing results for 
Search instead for 
Did you mean: 

implementation of a deep learning model on the STM32f446 board

Lamine
Associate

Is it possible to implement the model of human activity recognition mode zoo on the STM 32f446RE board Only the board and one sensor are used.Is it feasible or not?

2 REPLIES 2
Pavel A.
Evangelist III

Possible, with a certain degree of accuracy and number of creatures in the zoo.

 

what concerns the implementation in the card I was able to do but I can not give a demonstration, is there a template that i can implement to demonstrate