2024-11-24 6:06 AM
Hi everyone,
I'm trying to integrate st_yolo_lc_v1_192 pretrained model to my project on STM32H750 MCU.
I'm new to the framework and AI tech.
I see the output shape is 12x12x30 which I know the 12x12 means there are 12x12 grids. What I don't know is the '30', does that mean 5 * [x, y, w, h, confidence, class] ?
and do I need to apply an activation function to these values?
Thanks!
Solved! Go to Solution.
2024-11-25 12:16 AM
Hi,
Indeed 30 is 5 * [x, y, w, h, confidence, class] because by default st_yololc_v1 has 5 anchors.
To decode the raw output of the model we use this function:
https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/e5361e76f8427b0907b67d9815101d05c32e7407/object_detection/src/postprocessing/tiny_yolo_v2_postprocess.py#L12
and then you need to apply non max suppression, an example can be found here:
https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/e5361e76f8427b0907b67d9815101d05c32e7407/object_detection/src/postprocessing/tiny_yolo_v2_postprocess.py#L104
2024-11-25 12:16 AM
Hi,
Indeed 30 is 5 * [x, y, w, h, confidence, class] because by default st_yololc_v1 has 5 anchors.
To decode the raw output of the model we use this function:
https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/e5361e76f8427b0907b67d9815101d05c32e7407/object_detection/src/postprocessing/tiny_yolo_v2_postprocess.py#L12
and then you need to apply non max suppression, an example can be found here:
https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/e5361e76f8427b0907b67d9815101d05c32e7407/object_detection/src/postprocessing/tiny_yolo_v2_postprocess.py#L104