2025-01-02 05:55 AM - edited 2025-01-03 03:21 PM
This ONNX model is compiled with a standard MCU and runs on it (both with and without quantization). However, I encounter the following error when using the Neural-ART Accelerator NPU (both with and without quantization):
INTERNAL ERROR: Scale, zero-point, and quantizer must be set simultaneously.
It seems to me that all the model's onnx operations are supported (https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_operator_support.html)
Solved! Go to Solution.
2025-01-09 12:27 AM
Hello @Fra_ ,
After investigation, the issue is caused by the equal layer. We opened a ticket internally to fix it.
Have a good day,
Julian
2025-01-06 08:17 AM
Hello @Fra_,
Can you share the model in a .zip file?
Have a good day,
Julian
2025-01-06 11:34 AM
2025-01-09 12:27 AM
Hello @Fra_ ,
After investigation, the issue is caused by the equal layer. We opened a ticket internally to fix it.
Have a good day,
Julian