cancel
Showing results for 
Search instead for 
Did you mean: 

Error Neural-ART Accelerator MCU: "INTERNAL ERROR: Scale, zero-point, and quantizer must be set simultaneously"

Fra_
Associate II

This ONNX model is compiled with a standard MCU and runs on it (both with and without quantization). However, I encounter the following error when using the Neural-ART Accelerator NPU (both with and without quantization):

INTERNAL ERROR: Scale, zero-point, and quantizer must be set simultaneously.

 

It seems to me that all the model's onnx operations are supported (https://stedgeai-dc.st.com/assets/embedded-docs/stneuralart_operator_support.html)

2 REPLIES 2
Julian E.
ST Employee

Hello @Fra_,

 

Can you share the model in a .zip file?

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Here the zip file