cancel
Showing results for 
Search instead for 
Did you mean: 

Error analysing LSTM model using X-Cube-AI: ""NOT IMPLEMENTED: Order of dimensions of input cannot be interpreted""

Lemanoise
Associate II

As stated, I have problem analyzing the ONNX model ported from a pytorch model. The code of the model is simple as follows:

 

class LSTM(nn.Module):

    def __init__(self, input_size, hidden_size, num_layers, num_output=1):
        super(LSTM, self).__init__()
        
        self.num_layers = num_layers
        self.input_size = input_size
        self.hidden_size = hidden_size
        self.num_output = num_output
        
        self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
                            num_layers=num_layers, batch_first=True)
        
        self.fc = nn.Linear(hidden_size, num_output)
        
    def forward(self, x, device='cuda'):
        
        ula, (h_out, _) = self.lstm(x)
        
        out = self.fc(h_out[-1])
        
        return out

 

 Netron vis:

Lemanoise_0-1734007590314.png

I will really appreciate any advice or workarounds. Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions
Julian E.
ST Employee

Hi everyone,

 

I did some test on my side and we currently only support LSTM with 1 hidden size and 1 layer. Something like: 

import torch
import torch.nn as nn

# Simple lstm that works

class LSTM(nn.Module):
    def __init__(self, input_size, hidden_size, num_layers, num_output=1):
        super(LSTM, self).__init__()
        self.num_layers = num_layers
        self.input_size = input_size
        self.hidden_size = hidden_size
        self.num_output = num_output

        self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
                            num_layers=num_layers, batch_first=True, bidirectional=False)
        

        self.fc = nn.Linear(hidden_size, num_output)

    def forward(self, x, device='cuda'):
        ula, (h_out, _) = self.lstm(x)
        out = self.fc(h_out[-1])
        return out

# If not 1 : error
# other parameter we can put anything
input_size = 10 
hidden_size = 1 
num_layers = 1 
num_output = 10  

model = LSTM(input_size, hidden_size, num_layers, num_output)

model.eval()

dummy_input = torch.randn(1, 128, input_size)

onnx_file_path = "simple_lstml.onnx"
torch.onnx.export(model, dummy_input, onnx_file_path, 
                  input_names=['input'], output_names=['output'])

 

I tried to stack multiple LSTM but I had no success. 

I am asking for more information, I will keep you updated

 

Have a good day,

Julian

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

10 REPLIES 10
Julian E.
ST Employee

Hello @Lemanoise,

 

Can you attach your onnx model in a .zip file please?

 

In the meantime, make sure you follow the conditions described in the ONNX Toolbox documentation concerning the LSTM: 

 

LSTM

Computes a multi-layer long short-term memory (LSTM) RNN to an input sequence (batch=1, timesteps, features)

  • category: recurrent layer
  • input data types: float32
  • output data types: float32

Specific constraints/recommendations:

  • stateless mode support only
  • fused activation: sigmoid
  • fused recurrent activation: sigmoid
  • return_state not supported
  • Only 1 input is allowed for LSTM; the others should be constant and placed into the initializers
  • layout=1 attribute is not supported

 

https://stedgeai-dc.st.com/assets/embedded-docs/supported_ops_onnx.html

 

Have a good day, 

Julian

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lemanoise
Associate II

Yeah sure, here is the onnx model. Thank you for your advice and I'll look into it as well. 

Hello,I have the same question.Do you slove this question?

No not yet, I hope ST staffs will check my model and give us further guidance. 

I read a answer. someone answer cubeai 10.0.0version slolve this question. but I not try yet.

I tried the X-Cube-AI 10.0.0 and also the new ST Edge AI Developer Cloud, they did not solve my problem. 

Julian E.
ST Employee

Hi everyone,

 

I did some test on my side and we currently only support LSTM with 1 hidden size and 1 layer. Something like: 

import torch
import torch.nn as nn

# Simple lstm that works

class LSTM(nn.Module):
    def __init__(self, input_size, hidden_size, num_layers, num_output=1):
        super(LSTM, self).__init__()
        self.num_layers = num_layers
        self.input_size = input_size
        self.hidden_size = hidden_size
        self.num_output = num_output

        self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
                            num_layers=num_layers, batch_first=True, bidirectional=False)
        

        self.fc = nn.Linear(hidden_size, num_output)

    def forward(self, x, device='cuda'):
        ula, (h_out, _) = self.lstm(x)
        out = self.fc(h_out[-1])
        return out

# If not 1 : error
# other parameter we can put anything
input_size = 10 
hidden_size = 1 
num_layers = 1 
num_output = 10  

model = LSTM(input_size, hidden_size, num_layers, num_output)

model.eval()

dummy_input = torch.randn(1, 128, input_size)

onnx_file_path = "simple_lstml.onnx"
torch.onnx.export(model, dummy_input, onnx_file_path, 
                  input_names=['input'], output_names=['output'])

 

I tried to stack multiple LSTM but I had no success. 

I am asking for more information, I will keep you updated

 

Have a good day,

Julian

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lemanoise
Associate II

Thank you! I have tried the one-layer case and it succeeded. Please keep sharing further information on multi-layer case if any :)

Julian E.
ST Employee

Hello  @Lemanoise ,

 

Using tensorflow, I could use multiple LSTM one after the other (which I did not succeed to do with pytorch).
It may be useful for you:

 

import tensorflow as tf
from tensorflow.keras.models import Model
from tensorflow.keras.layers import Input, LSTM, Dense


input_layer = Input(shape=(100, 2), batch_size=1)

lstm1= LSTM(32, activation='relu', stateful=True,return_sequences=True)(input_layer)

lstm2 = LSTM(32, activation='relu', stateful=True,return_sequences=True)(lstm1)

output_layer = Dense(units=3, activation='linear')(lstm2)

# Create the model
model = Model(inputs=input_layer, outputs=output_layer)

# Print the model summary
model.summary()

# Compile the model
model.compile(optimizer='adam', loss='mean_squared_error')


model.save('tf_lstm.h5')

 

Be careful to follow these instructions while using it:

JulianE_1-1734366676509.png

https://stedgeai-dc.st.com/assets/embedded-docs/keras_lstm_stateful.html 

 

Have a good day,

Julian


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.