cancel
Showing results for 
Search instead for 
Did you mean: 

Automatic Validation on target compilation problem

DenDanne
Associate II

Hello. I have made with ST Edge AI Developer Cloud a model and downloaded the whole project for STM32CubeIDE.

 

When I do Validate on desktop it works fine and I get expected results.

But Validate on target gives me a compilation error.

 

DenDanne_0-1730889104446.png

 

Building project 
Generating project 
Temporary project loaded 
Temporary AI configuration done 
Generating temporary project code 
Building project 
C:/ST/STM32CubeIDE_1.16.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/arm-none-eabi-gcc -c -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard  -DDEBUG -DUSE_HAL_DRIVER -DSTM32G491xx -D  -IDrivers/CMSIS/Device/ST/STM32G4xx/Include -IDrivers/CMSIS/Include -IDrivers/STM32G4xx_HAL_Driver/Inc/Legacy -IDrivers/STM32G4xx_HAL_Driver/Inc -IInc -IMiddlewares/ST/AI/Inc -O3  -Wall -fdata-sections -ffunction-sections Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.c -o Debug/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.o 
<command-line>: error: macro names must be identifiers 
In file included from Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal_rcc.h:27, 
                 from Inc/stm32g4xx_hal_conf.h:212, 
                 from Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal.h:29, 
                 from Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.c:35: 
Drivers/STM32G4xx_HAL_Driver/Inc/stm32g4xx_hal_def.h:29:10: fatal error: stm32g4xx.h: No such file or directory 
   29 | #include "stm32g4xx.h" 
      |          ^~~~~~~~~~~~~ 
compilation terminated. 
make: *** [Makefile:75: Debug/Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal.o] Error 1 
Automatic build and run failed

 

So it does not compile successfully with the no such file or directory for stm32g4xx.h
I have made zero changes to the downloaded project from Developer cloud. And when I try and compile the project myself, it does so successfully. 

 

10 REPLIES 10

Pinagadi_Meghana_0-1741859884912.png

i got the same error.... what should i doo...
i didnt use any edge ai developer cloud... instead i did using mx... but the same error is displaying there...??
please help me through this...