2025-01-01 11:57 PM - edited 2025-01-02 12:01 AM
Hello, ST community members, I am trying to port an onnx model to STM32H743VITx through X-CUBE-AI. When analyzing the network, the following error message appears:
"TOOL ERROR: Error in computation of shapes"
I don't know if it is because some layers in the network are not supported by the tool, or maybe because my network is two branches and then aggregated, but I can use the same single-branch model to pass the analysis. I uploaded my model structure in the form of a picture, hoping to get your help, thank you!
2025-01-06 6:11 AM
Hello @lc_guo,
You can find the list of supported layers here:
https://stedgeai-dc.st.com/assets/embedded-docs/supported_ops_onnx.html
Can you share your model in a .zip file please?
Else, can you open a git bash where stedgeai is located and type:
Then share the results.
Have a good day,
Julian
2025-02-27 4:39 AM
Hello @Julian E. , sorry to see your reply now.
I appreciate your reply, my model has been presented in the form of a zip package in the attachment, I am very much looking forward to your reply again!
2025-03-13 6:53 AM - edited 2025-03-13 6:57 AM
Hello @lc_guo ,
Sorry for the late answer, I forgot to message you.
Using the version ST Edge AI Core v2.0.0-20049, when doing a generate, the model in the zip in your last message works.
You can check your version using the command: stedgeai.exe --version.
(it should be located in C:\Users\YOUR_USERNAME\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\10.0.0\Utilities\windows)
I think that you are using the X Cube AI GUI (which calls the stedgeai core in background).
If you still have issue, I would suggest to try to uninstall and install the X Cube AI and if it still not works ,then uninstall X Cube AI, then download the ST Edge AI Core () and download X Cube AI again.
This time, CubeAI will use the standalone version of ST Edge AI. In theory they are the same.
Tell me if you need anything,
Have a good day.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.