2024-08-15 08:08 AM
It's a shame that the serial emulator in AI Studio only supports a COM port as input and not an offline .csv file of recorded data, as it's not always possible to have access to a live stream.
I've noticed as well that the COM port options don't seem to include COM ports that have redirected from a host computer when using Remote Desktop (but TeraTerm appears to do this OK).
2024-08-16 12:53 AM
It should be noted btw that you can use an input file to the command line emulator that you download from the GUI, it's just that you can use a file as an input to NanoEdge AI Studio.
2024-08-16 02:53 AM
Hello @GMeta.1,
If you want to test a library with offline file like .csv or .txt, you can select a library in validation and do an "Experiment". It's true that experiments results don't give much information for the moment, but we are aware of it and we are working on it.
Experiments are made to test and compare one or multiple libraries with offline files and the serial emulator is made to test a single library with serial.
Thank you for your remark about COM ports on remote desktop, I will notice the development team about this.
Have a good day,
Julian