cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to ''flash'' code to target

Raghu Rajappa
Associate
Posted on July 27, 2017 at 14:00

Hi,

I am using a SPC560C50L3 controller on a SPC560BADPT100S MINIMODULE board which sits on the XPC56XX EVB Motherboard. Power supply checked, jtag driver checked. The JTAG used is from PLS USB/JTAG Adapter for SPC5XXX. 

Using a sample application (CAN application), I could manage to build the code. But from here on, I tried to read the manual to use the JTAG debugger but I could not successfully flash code. Another thing I notice while using UDE STK4.8 version, is the Target names (in Select target configuration) DO NOT match any of the names (name of controller, minimodule or the motherboard). From this what I understand is I do not have a target configuration file, specific to the board in use. 

How can I solve this?? Any help is appreciated.  

#spc5 #pls #spc5-studio #jtag
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on August 09, 2017 at 17:02

Hello Raghu ,

Sorry for the late answer,

in PLS UDE tool 4.8, you should create your workspace from scratch 

(cf Screenshot)

0690X00000607lwQAA.png

   Best regards

               Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee
Posted on August 09, 2017 at 17:02

Hello Raghu ,

Sorry for the late answer,

in PLS UDE tool 4.8, you should create your workspace from scratch 

(cf Screenshot)

0690X00000607lwQAA.png

   Best regards

               Erwan