cancel
Showing results for 
Search instead for 
Did you mean: 

There exist an example for SPC58EC-DISP that I can use in order to send UDP message from SPC58EC-DISP via Ethernet without include FreeRTOS Component?

VNava.1
Associate III

Hi community!

my name is Vincenzo,

I am looking, if any, for an example application that would help me understand how to send UDP messages from the SPC58EC-DISP board over Ethernet.

For the moment I have found an interesting application that allows me to ping the SPC58EC-DISP from my PC, but I'm not being able to do anything else. I noticed that there are demos available inside this application such as Simple TCP Echo Server, but I have not been able to get it to work. There is some documentation about it? besides AN5413.

Moreover, I would like to know if it possible to create the Ethernet socket to send a UDP message without using the FreeRTOS Component RLA component?

Thanks in advance for your support!

Vincenzo

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.

These components are dependent on FreeRTOS.

You need to recreate from scratch the Ethernet socket.

Best regards

Erwan

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Hello ,

There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.

These components are dependent on FreeRTOS.

You need to recreate from scratch the Ethernet socket.

Best regards

Erwan