2026-02-10 2:53 AM - edited 2026-02-10 9:20 AM
Dear Community,
I have a general question. I wanted to use C++ classes in SPC5 Studio to get a cleaner project structure.
For this, I changed main.c to main.cpp and included the C headers using extern "C". I also enabled the C++ linker in the Platform Component RLA.
The project builds without any issues, but the parsing errors in the editor are extremely annoying. A lot of the code is marked in red even though it compiles fine.
Does anyone know what setting I need to adjust to get rid of all these unresolved reference errors in the parser (i presume...)?
Kind regards,
TKorn
Solved! Go to Solution.
2026-02-13 7:00 AM
Hello Tkorn ,
It is a CDT Issue .. i recommend to index with Gcc power-pc vle in plugins directories (gcc powerpc vle section)
or ignore the errors in Errors section
it is not so easy comparing vscode.
Best Regards
Erwan
2026-02-10 9:21 AM
Hello again,
I managed to find the problem, it is the indexing.
Unfortunately i didn't manage to solve to problem.
Can anyone help?
Kind regards
TKorn
2026-02-12 11:55 PM
Hello, can anybody help?
2026-02-13 7:00 AM
Hello Tkorn ,
It is a CDT Issue .. i recommend to index with Gcc power-pc vle in plugins directories (gcc powerpc vle section)
or ignore the errors in Errors section
it is not so easy comparing vscode.
Best Regards
Erwan