cancel
Showing results for 
Search instead for 
Did you mean: 

SR6G7 Stellar BCS handshake and Custom Boot Manager

mesutozi
Associate

I would like to know, in the Stellar SR6G7, whether the BCS code will execute first or if we can configure a custom Boot Manager to execute first. Since I need to run secure boot with HSM, I want to configure the Boot Manager for PLL clock initialization and run the HSM first. Then, the BCS will execute the handshake with the HSM. Is this possible in the SR6G7, or will the BCS handle initialization and perform the handshake with the HSM during startup before any custom Boot manager?

1 REPLY 1
C.A-T.
ST Employee

Hi,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.