cancel
Showing results for 
Search instead for 
Did you mean: 

SPCSetRunMode not return ......

guo qiang
Senior
Posted on April 13, 2017 at 10:27

SPCSetRunMode not return ......

board:

Discovery Plus Kit for SPC56 L line - with SPC56EL70L5 MCU

my step:

file->new sp5 studio Application wizard->

select

Discovery Plus Kit for SPC56 L line - with SPC56EL70L5 MCU

0690X00000606PiQAI.png

click generate button and click build button

0690X00000606kdQAA.png

program FLASH and debug...

Has been parked here....

0690X00000606kxQAA.png

I didn't changed any code...

0690X00000606l2QAA.png

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on April 14, 2017 at 13:00

1.Disconnect 

  

power and debugger , 

2.

connect power 

again.  app can not run.

This image represents the value of the PC when the program is not running

0690X00000606ZhQAI.png
Posted on April 14, 2017 at 13:05

0690X00000606m1QAA.png

I guess it's a configuration problem, but I don't know how to set it up to get the power to run

Posted on April 14, 2017 at 13:10

My English is very bad, I don't know if you can understand what I mean

Posted on April 14, 2017 at 14:05

Hello Guo ,

i am still waiting your Installation details

The hardware has not found a valid Boot ID in any flash memory boot locations

the device is fetching the code 0xFFFFC000

You have not flash the firmware, please flash the firmware by using LOAD PROGRAM in PLS

Anyway, for your information , SPC5Studio 5.3.0 is available.

You can update by Update site or Marketplace

we have corrected all the debug.wsx (it is compliant for PLS 4.8.2)

Use PLS 4.8.2 for to debug and flash.

                    Best regards

                                                                  Erwan

Posted on April 17, 2017 at 08:40

i am installed SP5Studio 5.3.0 and PLS 4.8.

that is ok.

Posted on April 17, 2017 at 10:52

I do through the '' load Program steps '', download the Program. 

0690X00000606k5QAA.png0690X00000606k6QAA.png

After  Disconnect 12V power , after a while....

I connect 12V Power and debugger.

look the memory  dialog

0690X00000606k0QAA.png

the memory address 0 value is 0x015A0000.

the pc value is 0xFFFFC0000

0690X00000606mjQAA.png

My PLS version is 4.8 demo verison. no input license.This causes?

Posted on April 17, 2017 at 14:01

The problem has been solved.

PA4 connect to GND. connect 12V power again.ALL GOOD~

TKX U Very much�?�?

Yvin.Erwan

Posted on April 17, 2017 at 14:01

The problem has been solved.

PA4 connect to GND. connect 12V power again.ALL GOOD~

TKX U Very much�?�?

Yvin.Erwan

.

Matthew Richardson
Associate II
Posted on January 22, 2018 at 11:03

I had this same issue, but it really had to do with the fact that I had older debug.wsx that didn't match the software version for the PLS I was using, which was 4.8.2.  Ensure that your PLS is updated and that SPC5Studio is updated (.wsx that came with 5.7.1 is aligned with PLS UDE 4.8.2).

Posted on January 24, 2018 at 09:42

Hello Matthew ,

You can recreate a debug.wsx from scratch by using new workspace in PLS UDE.

0690X00000609TMQAY.png0690X00000609TNQAY.png

Anyway, if you have an crash issue after configuring your clock.

i recommend you to check R13 and PC in the Core registers.

it will give a nice a nice clue where the problem happenned.

    Cordialement

                   Erwan