2024-08-14 8:11 AM
I am currently using an SPC56P chip for my application. But I do not have an debugger probe for it which is compatible with SPC5Studio. So my question is:
1. Is SPC5-UDESTK-EVAL the only debugger probe that is compatible with SPC5Studio ? Or are there any other SPC5Studio compatible debugger ?
2. Is there any other IDE, that will allow to use the Segger J-Link as debugger for SPC56P chip ?
3. The webpage of SPC5-UDESTK-EVAL suggests it being NRND (not recommended for new design), so is there a newer model available instead of it for SPC5Studio ?
I have tried SPC5Studio and AutoDevKitStudio and I think both are not compatible with J-Link.
Solved! Go to Solution.
2024-08-20 5:26 AM - edited 2024-08-23 2:00 AM
SPC5Studio and AutoDevKitStudio do not support SPC56 Family with :
https://www.segger.com/supported-devices/st/spc56
i recommend to use https://www.st.com/en/development-tools/spc5-udestk.html
Best regards
Erwan
2024-08-20 5:26 AM - edited 2024-08-23 2:00 AM
SPC5Studio and AutoDevKitStudio do not support SPC56 Family with :
https://www.segger.com/supported-devices/st/spc56
i recommend to use https://www.st.com/en/development-tools/spc5-udestk.html
Best regards
Erwan
2024-08-22 6:10 AM
Also another follow up question with respect to AEK-MCU-SPC5LNK, When will it be ready to use with SPC56 ? Is there any estimated time ?
2024-08-23 2:04 AM
Hello ,
AEK-MCU-SPC5LNK (FTDI Chipset)should work with OpenOCD (SPC58 only)
AEK-MCU-SPC5LNKU (FTDI Chipset) should work with UDE PLS (SPC56,SPC57 and SPC58)
Best Regards
Erwan