2015-09-18 4:51 AM
Dear All ,
SPC5Studio 3.7.0 is available*** Highlights ***- SPC563Mxx RLA (Register Level Access) drivers for Monaco, with sample applications and related documentation - EEPROM emulation software, with sample applications and related documentation - Saving and restore Pin map wizard settings - Added FlexCAN2 support for SPC56EL70L5 MCU (Leopard)- Marketplace features enabled with official http web addressBugs fixing:- fixed a problem on the Pinmap Wizard for SPC56ECxx MCU (Bolero 3M) - fixed issue on FlexCAN1 on SPC563Mxx MCU (Monaco)- watchdog threshold issue solved for ADC driver for SPC56P/L/B/D/C MCU - fixed issue for SCI driver for SPC56M/A MCU - Minor cosmetic changes for nil OS, CRC, eTimer2 test applications for SPC56L/B/D/C MCU- Several bugs and improvements, please refer to https://my.st.com/public/STe2ecommunities/mcu/Lists/SPC5%20Studio/AllItems.aspx(when the forum will be available)*** Notes ***- Make sure to read the SPC5Studio Users Guide and ComponentsWriters Guide inthe help section.Enjoy SPC5Studio,The SPC5Studio Team.2015-10-27 11:03 PM
Hi,
where to download the latest version v3.7.0?The ST.com still display v3.5.2015-10-28 1:02 AM
Hi Michael,
please note that SPC5Studio is delivered in two different ways, depending on the changes. Major changes are delivered in a full installer that you can download from ST.com, while less important changes are delivered through Eclipse update site mechanism.New users have to download first the latest major version (in your case version 3.5), then update it (each time SPC5Studio is launched a check for updates is done, that you can accept or refuse).Hope this helpsBest regardsPhilippe