cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5STudio 3.4.0 is available !

Erwan YVIN
ST Employee
Posted on January 26, 2015 at 16:57

SPC5STudio 3.4.0 is available !

Dear Users,

The 3.4.0 release is now available on the update site.

Here are is the change log

SPC5STUDIO CORE :

- Patch mode: newly created project is already patched

- Implementing invisible groups

- Allow user to patch components/lib/ files: V2

- Patch mode : patch.xml to be hidden / Default / Grey Decorators

- Implement Hidden properties

SPC5STUDIO Repository :

- Create NIL RTOS SPC560Bxx Test Application for Discovery

SPC5STUDIO Pinmap :

- Unable to Set more than 10 pin in PinMap Wizard

SPC5-HAL :

- CAN Naming convention : Change the id number of Filter Settings

- The message buffers Tx/Rx Configuration in CAN module are fixed

- The incorrect registers bits definitions and driver data structures and types in hal_lld.h head file

- eMIOS channels 1,3,5,6,2,4,11,13 are not usable for ICU

- PWM/ICU functions on eMIOS

NIL RTOS :

- New feature for SPC560Bxx

We wish you a happy usage.

The SPC5Studio team.

#latest-release
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
5 REPLIES 5
ssk
Associate II
Posted on January 28, 2015 at 15:05

Hello Erwan,

From where can I download the latest release? I tried from 'spc5.drive.cloudforge.com/projects/spc5releases/' but I am not finding it here.

What is the update site?

Please help. Thanks in advance.

Mike.

Erwan YVIN
ST Employee
Posted on January 30, 2015 at 11:06

Hello Mike ,

You have to use the menu :

Help ==> Install New software

and pick on SPC5Studio Update site

do not forget to put your proxy settings in Windows ==> Preferences (Network)

                Best Regards

                             Erwan

ssk
Associate II
Posted on January 30, 2015 at 12:02

Hello Erwan,

How to download in case the PC is not having the internet connection? I am using SPC5Studio on a lab PC where internet connection is not available.

Thanks.

Mike.
Erwan YVIN
ST Employee
Posted on February 06, 2015 at 15:25

Hello Mike ,

in the next days , we will send you a direct link to download the patch by ZIP File

Best regards

                Erwan

ssk
Associate II
Posted on February 09, 2015 at 06:57

Thanks Erwan. I am eagerly waiting for the link!! Look forward to receive it at the earliest.

Thanks.

Mike.