2020-08-05 08:22 AM
Hello, we bought 3x SPC 582B-DIS Eval Boards. I tested the first one with one of the examples provided in the SPC5 Studio successfully ~2 months ago. Last week I tried to put it into operation again but in Windows it's not recognized ("unknown usb device (port reset failed)").
I thought that this might have been due to ESD issues or mechanical stress during storage, so I tried the second Eval Board which was working perfectly at the beginning. This time I was more careful (Operation and storage only in air-conditioned ESD lab).
Nevertheless, the Board worked less and less over time while testing several examples (always lost USB connection during operation - needed to reconnect USB). Now the board is in the same state (not being recognized by Windows), no matter how often I plug it in and out.
Especially for the second board I took care that no mechanical or electrical stress (not even electrical measurements) were applied.
In the device manager, it's displayed as "unknown usb device (device descriptor request failed code 43)"
I tested
Is this a known problem? I'm fearing that a PLS UDESTK Debugger will behave similar.
Thank you for any help!
I'm going to test my third (and last) board now...
2020-08-10 10:37 AM
Yes, the third board also stopped working after few hours.
Now I've got one question:
According to the board's schematics, the FTDI2232 is connected to 5V:
According to the Data sheet of the FT2232 , its absolute maximum rating is ~3.6V.
Especially for VPhy it's written " Note that this cannot be connected directly to the USB supply. A +3.3V regulator must be used. "
Mounting the jumpers JP3 back to its initial position rises the voltage from 3.3V to 5V at TP100 (LVDD). Unfortunately I have no board left now to test whether this is the cause of the problem...
2020-08-13 02:15 AM
Hello , I have forwarded this question to the PCB manager.
Best regards
Erwan