2021-02-07 04:43 PM
I have bought the SPC582B-DIS EVB from Mouser. (SPC582B-DIS STMicroelectronics | Mouser Korea, Republic of)
However, this product doesn't work normally. I think there is a problem with FDTI Dirver chip as below.
So, I asked Mouser for a refund. However, they asked me to confirm from ST that there was a problem with the product. Please, help me for a refund.
Thank you.
Solved! Go to Solution.
2021-02-15 06:06 AM
Hi,
the suspect is that the issue is in the FTDI chip. There could be a programming issue. You should refer to PLS for checking the FTDI programming. Otherwise, you have to ask the board replacement.
Regards,
Luigi
2021-02-09 01:36 AM
Hi,
this error message could occur if there is a problem on the FDI connection or if you have selected a wrong debug configuration script. Please, could you specify which version of the PLS debugger are you using and which target configuration are you using?
Regards,
Luigi
2021-02-09 04:33 PM
HI,
We have three SPC582B-DIS, one is operating normally under the same conditions, and the other 2EA is problematic.
We have used a PLS debugger built in SPC582B-DIS.
UDESTK Version i s 5.02.04.
Thank you.
2021-02-09 10:45 PM
2021-02-14 05:10 PM
Hi,
I set the target configuration well.
Please, refer to the revision number of board. (Rev 1.1)
Thank you.
2021-02-15 06:06 AM
Hi,
the suspect is that the issue is in the FTDI chip. There could be a programming issue. You should refer to PLS for checking the FTDI programming. Otherwise, you have to ask the board replacement.
Regards,
Luigi
2021-02-17 04:20 PM
Hello Zambrano,
Hope you are doing well
I am working for Mouser Electronics and received the issue from our customer as above.
In regards to 2 pcs of part#SPC582B-DIS which seems to have programming issue, could you please advise whether the parts will be returned to ST or can be scrapped if we would like to proceed sending replacement or refund? Please advise. Thanks.
Best Regards,
Dan Lee
2021-02-21 06:03 PM
Hello Zambrano,
Any update? Please advise if we would like to refund 2 pcs of part#SPC582B-DIS customer received, theses will be returned to ST or can be scrapped by themselves. Thanks.
Best Regards,
Dan Lee