cancel
Showing results for 
Search instead for 
Did you mean: 

SPC58 RM: How should we start DCF records writing? If there is any RESERVED area after DCF Start?

Veniamin BELYAEV
Associate II

In the document RM0407 Rev.5 there are two different memory maps on pages 87 and 717.  According to p.236 we have to write 2 DCF records (16 bytes) in one program operation, but now we have RESERVED area after DCF Start record area. How we should write start record properly? The screenshots are attached.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Giuseppe DI-GIORE
ST Employee

Using Reference Manual 407 ver.5, the table to use is Table 11 at page 87

To clarify:

  • overall DCF area starts at offset 0x300 where there is the DCF Start Record (64 bit)
  • from 0x308 to 0x36F is Reserved
  • Customer DCF records area starts at offset 0x370

In summary, customer should start writing DCF records at offset 0x370

Regards,

Giuseppe

View solution in original post

2 REPLIES 2
Veniamin BELYAEV
Associate II

The address highlighted in the picture attached is not same as 0x00400300 or 0x00400370 described before. This address is part of LifeCycle slot 1.

Giuseppe DI-GIORE
ST Employee

Using Reference Manual 407 ver.5, the table to use is Table 11 at page 87

To clarify:

  • overall DCF area starts at offset 0x300 where there is the DCF Start Record (64 bit)
  • from 0x308 to 0x36F is Reserved
  • Customer DCF records area starts at offset 0x370

In summary, customer should start writing DCF records at offset 0x370

Regards,

Giuseppe