2020-10-09 2:56 AM
Hallo everyone.
I am evaluating this platform and I got it to work with the UDE STK debugger env.
unfortunatley when I shutdown my laptop at the end of the day, it seems to loose all the driver settings.
The morning after when I try to connect to the boar dit gives me this error message:
Message from component 'PpcJtagTargIntf' :
Can't connect target !
Message from component 'PpcJtagTargIntf' :
No JTAG client found !
Please check:
- target power supply
- JTAG cable connection
- target configuration
I am on W10 Pro x64.
I connect the eval board USB cable to the dock (but it has same behavior even if I use the laptop's own ports)
The drivers for FTDI and PLS USB JTAG adapter are installed and configured in device manager settings:
I don't like having to reinstall the UDE STK 5.0 every day...
Has anyone faced the same problem? how did you fix it (if ever)?
Thanks in advance
Maurizio
Solved! Go to Solution.
2020-10-12 2:51 AM
Greetings Every1,
I answer to myself: by disabling in WIndows Device Manager one of the two interfaces, the debugger now works OK.
Right-click, select disable.... (you can re-eanble at anytime)
2020-10-12 2:51 AM
Greetings Every1,
I answer to myself: by disabling in WIndows Device Manager one of the two interfaces, the debugger now works OK.
Right-click, select disable.... (you can re-eanble at anytime)