2021-11-27 10:36 PM
I have 3 documents (DocID14642 Rev 12, Doc ID 13850 Rev 6, DocID14499 Rev 9) from the SPC563M64L5 microcontroller.
Is there a complete datasheet other than these 3 documents from this microcontroller? And if so, what is the method of preparation?
I want to have ports and pin numbers. Information such as clock, commissioning of various microcontroller units, registers and all the necessary information to set up and work with this microcontroller.
2021-11-29 02:16 AM
You will find all relevant information on the website of the SPC563M64L5, e.g. the datasheet (your screenshot on the left) and the reference manual (your screenshot on the right).
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-11-29 02:36 AM
I want the number of pins and ports of the SPC563M64L5 microcontroller. Please guide me.
2021-11-29 03:02 AM
As already mentioned, AN3190 does not apply here.
The GPIO are handled by the SIU and the datasheet says in section 2.3.7:
Regards
/Peter
2021-11-29 03:34 AM
The specifications of the pins and ports are specified in the SPC560P50L5 microcontroller, but it is not clear in the SPC563M64L5 microcontroller. Please guide me.
2021-11-29 03:45 AM
The specifications of the pins and ports are specified in the SPC560P50L5 microcontroller, but it is not clear in the SPC563M64L5 microcontroller. Please guide me.
2021-11-29 04:14 AM
I don't understand what you are looking for exactly - the marked pins AN [25] and AN [27] are described in table 4, page 52 of the datasheet, e.g.:
What do these pins have to do with the SPC560P50L5?
Regards
/Peter
2021-11-29 04:25 AM
Very well, I mean more clearly. I want to know the port name and pin number of the SPC563M64L5 microcontroller. For example, to know where the port B or port E are, and also to know how many pins each port has and which microcontroller bases are the numbers of those pins.
2021-11-29 04:42 AM
There is no port B or port E, there are just GPIOs. The datasheet says at the bottom of table 6:
GPIO[n]:
Configurable general purpose I/O pins. Each GPIO input and output is separately controlled by an 8-bit input (GPDI) or output (GPDO) register. Additionally, each GPIO pins is configured using a dedicated SIU_PCR register.
The GPIO pins are generally multiplexed with other I/O pin functions.
The registers GPDI and GPDO are described in the reference manual, sections 15.8.15 and 15.8.16.
Regards
/Peter
2021-11-29 05:02 AM
But in the SPC5Studio software it is possible to configure through the type of port and pin number.