2014-10-08 6:56 AM
Hello,
If I am using the command ''asm volatile (''nop'');
'', how long should the controller need to execute this command?
I ask this question because I have tried to use it as an indicator for the system clock. Currently, I am using the SPC560D discovery board and my clock source is the FMPLL, configured for a clock of 48MHz. The SPC5-UDESTK and UDE Visual Platform shows me an execution time of 208ns for this command. This seems too much for me for a system clock of 48Mhz. Shouldn´t it be around 10ns? To do another test, I used the internal 16Mhz RC as system clock. The strange thing is, that the execution time for this command is exactly the same. Best regards, Patrik2014-11-14 7:08 AM