Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

eMIOS overflow callback and frequency range

Posted on October 19, 2015 at 12:20Hello, when I was working on SPC56EL with older SPC5 Studio versions, the overflow callback was called only when the internal counter was overflowing. This was perfect to detect too low frequency which can't be mea...

Updates

Posted on November 10, 2015 at 15:44Hello everybody,I tried to update SPC5 studio but i got the error ''No repository found containing:''on every update package.Trying to fix this problem I accidentally erased repositories.Now i need to know what si...

SPC5UDESTK - Checksum

Posted on October 07, 2015 at 14:48I am using Universal Debug Engine v4.02.07 for programming the flash with SPC560D MCU with PLS USB/JTAG adapter. Where can I find the checksum value for the obj file (.elf or .hex or .out)? Which menu of the tool h...

ssk by Associate II
  • 2111 Views
  • 4 replies
  • 0 kudos

SPC5Studio 3.7.0 is available !!!

Posted on September 18, 2015 at 13:51Dear All ,SPC5Studio 3.7.0 is available*** Highlights ***- SPC563Mxx RLA (Register Level Access) drivers for Monaco, with sample applications and related documentation - EEPROM emulation software, with sample app...

SPC560B LinFlex_1 slave mode initialization

Posted on October 20, 2015 at 14:44Hello all, I’m trying to initialize the LinFlex LINFLEX_1 module of the SPC560B Bolero. Unluckily I’m running into problems writing the  LINFLEX_1.LINCR1 register. Specially I’m unable to write the LINFLEX_1.LINCR1...

dominik2 by Associate II
  • 1193 Views
  • 2 replies
  • 0 kudos

FlexCAN not work

Posted on October 10, 2015 at 09:57Hi,I am testing SPC560P50L5 with spc5_studio, the built-in example for FlexCAN is loopback test. When I disable loopback and enable supervisor mode, there is nothing on the CAN_TXD pin. I do not know the problem, a...

Using CAN on SPC560B-DIS

Posted on November 19, 2014 at 16:24Hello,I am trying to make a simple project that for a start can send a single CAN frame.I am using the SPC560B-DIS evb without any CAN board (will connect later on my own converter).I took a CAN sample  from other...

srosen by Associate II
  • 5806 Views
  • 11 replies
  • 0 kudos

where to find low level driver for SPC5604B ?

Posted on October 06, 2015 at 09:27HI,We are going to use SPC5604B for the coming project, and have  installed SPC5Studio, and also imported all the components, but still dont find low level drivers for SPC5604B, but found lld for SPC5604P, but seem...