2014-10-21 09:35 AM
Can't seem to connect to the SPC560B-DIS via USB or JTAG-USB (SOC5-UDESTK) to the UDE debugger. UDE does not list the device SPC560B54L5. UM1672 User Manual (Table 3) mentions some ''jumper'' states that are in actual fact not jumpers and would require soldering to change configuration.
Can someone help? #spc5studio2015-01-21 08:35 AM
Good news ;)
Best regards Erwan2015-06-01 08:04 AM
We are using the spc560B60L3 100 pin package in adevelopment project. We need to use 4 LINflex interfaces.
In the data sheet, it is mentioned that it supports 4 LINs.Can we use LIN4 and LIN5 or it only supports LIN0 up to LIN3?
Thanks2015-06-05 05:16 AM
Same issue as
Best Regards Erwan