Skip to main content
Patriks
Senior
May 7, 2015
Solved

[solved] eTimer input capture mode SPC56EL

  • May 7, 2015
  • 2 replies
  • 762 views
Posted on May 07, 2015 at 10:57

Hello,

I would like to use the input capture functionality of eTimer on SPC56EL. This is my eTimer configuration:


ETIMER_0.CHANNEL[0].CTRL1.B.PRISRC = 0b11000; 

ETIMER_0.CHANNEL[0].CTRL1.B.SECSRC = 0b00010; 

ETIMER_0.CHANNEL[0].CTRL1.B.CNTMODE = 0x3; 

ETIMER_0.CHANNEL[0].CTRL1.B.LENGTH = 0x0; 

ETIMER_0.CHANNEL[0].CTRL1.B.DIR = 0x0; 


ETIMER_0.CHANNEL[0].CTRL2.B.OUTMODE = 0x3; 

ETIMER_0.CHANNEL[0].CTRL2.B.OEN = 0x1; 


ETIMER_0.CHANNEL[0].CCCTRL.B.CLC2 = 0x5; 

ETIMER_0.CHANNEL[0].CCCTRL.B.CLC1 = 0x2; 

ETIMER_0.CHANNEL[0].CCCTRL.B.CMPMODE = 0x0; 

ETIMER_0.CHANNEL[0].CCCTRL.B.CPT2MODE = 0x1; 


ETIMER_0.CHANNEL[0].INTDMA.B.ICF2IE = 0x1; 

ETIMER_0.CHANNEL[0].INTDMA.B.CMPLD1DE = 0x1; 

ETIMER_0.CHANNEL[0].INTDMA.B.CMPLD2DE = 0x1; 


ETIMER_0.DREQ[0].R = DREQ_ENABLED | DREQ_CMPLD1_CH0; 

ETIMER_0.DREQ[1].R = DREQ_ENABLED | DREQ_CMPLD2_CH0;

The primary input source is the bus clock, the secondary input source is an external signal. The counter counts up with every rising edge of primary source when the secondary input is high. Additionally, I am using the compare load function to reload the compare values with DMA. Anyway, doesn´t matter because this part works fine. The counter runs up when secondary input is high and reloads the compare values. According to my configuration I expected that the eTimer captures falling edges of the secondary input source (my external signal) and stores the corresponding counter values to the CAPT_2 register. But the capture of falling edge isn´t working. Can anyone tell me if something is missing in my configuration or what I have to do to use the capture functionality? Best regards, Patrik
    This topic has been closed for replies.
    Best answer by Erwan YVIN
    Posted on May 29, 2015 at 14:44

    Hello Patrik ,

    Your configuration seems to be  ok.

    Did you arm the capture ?

    ARM - Arm Capture

    Setting this bit high starts the input capture process. This bit can be cleared at any

    time to disable input capture operation. This bit is self cleared when in one shot mode

    and the enabled capture circuit(s) has had a capture event(s).

    1 = Input capture operation as specified by the CPT1MODE and CPT2MODE bits is

    enabled.

    0 = Input capture operation is disabled.

       Best Regards

                       Erwan

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    May 29, 2015
    Posted on May 29, 2015 at 14:44

    Hello Patrik ,

    Your configuration seems to be  ok.

    Did you arm the capture ?

    ARM - Arm Capture

    Setting this bit high starts the input capture process. This bit can be cleared at any

    time to disable input capture operation. This bit is self cleared when in one shot mode

    and the enabled capture circuit(s) has had a capture event(s).

    1 = Input capture operation as specified by the CPT1MODE and CPT2MODE bits is

    enabled.

    0 = Input capture operation is disabled.

       Best Regards

                       Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Patriks
    PatriksAuthor
    Senior
    June 8, 2015
    Posted on June 08, 2015 at 15:06

    Hello Erwan,

    That's it, now it works! Thanks for your help!

    Best regards,

    Patrik